element14 is now stocking Weller’s new hand soldering solution WXsmart
Weller’s WXsmart is the first all-in-one hand soldering platform offering total process control with maximum connectivity and traceability to support Internet of Things (IoT) standards

element14 is shipping the new-to-market WXsmart, an all-in-one smart hand soldering platform from Weller. A first of its kind solution, the WXsmart is designed to reduce downtime and increase productivity for all soldering, repair and rework applications.
The new WXsmart is the first-hand soldering station to bring smart productivity, connectivity, security and intelligent features in a space and energy saving design to the industry. The integrated all-in-one station acts as the brain of a workbench by consolidating all soldering applications with intelligent soldering tips and tools. WXsmart supports all Internet of Things (IoT) standards for full traceability with mobile-enabled remote-control access.
Global production is growing exponentially especially within the electronics, medical and aerospace industries as components become more powerful. Weller is meeting this demand with a new generation of Smart Tips that include an integrated chip in every soldering tip, providing new added-value features to operators.
These chips enhance the Weller soldering tip to offer greater precision and improve the collection of traceable data, such as using the soldering iron, temperature excursions and operation time by individual users. Lock functions make soldering processes repeatable and transparent.
Key features of Weller’s WXsmart all-in-one smart hand soldering platform, now available for fast delivery from element14, include:
- Process control – The locked parameter functions on tip allow users to achieve full process control and prevent defaults during the soldering process.
- Integrated data storage with built-in connectivity – Each smart soldering tip has integrated data storage with a unique individual serial number for full traceability and calibration history. This enables the built-in Total Process Control (TPC) intelligence to manage the complete soldering process from tip to station. The data gathered is not natively stored in the cloud. Instead, the platform enables customers to securely collect, store and use data to suit their application needs.
- Accurate data results with tip-offset function – The reference point of the sensor can be changed easily using the ‘Tip Offset’ function. This enables operators to efficiently achieve results with the highest degree of accuracy.
- Maximum precision and protection – The short tip-to-grip distance and optimised shape provide maximum precision during the soldering process. The RTUS smart soldering tips comply with MIL-SPEC and IPC industry standards (IPC - TM-650 2.5.33 Measurement of Electrical Overstress from Soldering Hand Tools). This provides maximum protection to the printed circuit board and components, achieving excellent results while keeping operating costs low.
- High compatibility – The platform can be used with the WXUPS MS Smart Soldering Iron and WXsmart Soldering Station, which automatically identifies each patented Weller RTUS cartridge tip. The RTUS smart cartridge tips can also be changed quickly, safely and efficiently without additional tools.
James McGregor, Global Head of Test, Tools and Production Supplies at element14 says, “As a leading global manufacturer of soldering solutions, Weller is well-known for pioneering innovative technology. The new WXsmart all-in-one smart hand soldering platform offers high performance and high repeatability that includes enhanced data capture for quality control, traceability and manufacturing efficiency.”
Weller’s WXsmart all-in-one smart hand soldering platform is available from stock at Farnell in EMEA, Newark in North America and element14 in APAC.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate