element14 launch Raspberry Pi based Design Competition for engineers and makers in China who are creative and dare to innovate
Innovative ideas and practical solutions are welcome! - closing date for initial ideas 27 October 2017
element14, the Development Distributor, has launched element14 Cup Raspberry Pi Creative Design Competition- in China looking for innovative or practical applications of the Raspberry Pi. Contestants have full creative freedom allowing them to design devices that meet any need – from home automation to industrial application and beyond. The only criteria that must be met is the inclusion of a Raspberry Pi 3 model B in the design.
The Raspberry Pi 3B is the latest offering from the Raspberry Pi Foundation. The new generation board is faster and more powerful than ever before and comes with built-in Wireless and Bluetooth connectivity. The Raspberry Pi 3 is built on a new QUAD Core Broadcom BCM2837 64bit ARMv8 processor (running an ARMv7 operating system) at 1.20GHz, a significant increase from 900MHz on the Raspberry Pi 2. It has improved power management and an upgraded switched power source up to 2.5 Amps to support more powerful external USB devices. With support for Bluetooth Low Energy and Wireless LAN, the Raspberry Pi 3 can support new and exciting application areas ‘out of the box’, such as IoT connectivity, streaming to Bluetooth headphones or speakers, Wi-Fi gateways and home cloud storage.
Contestants may also consider one of a range of add-on devices available from element14 that can be used with the Raspberry Pi 3 to speed up design or broaden the application of the device.
-
The Raspberry Pi SenseHAT attaches to the top of a Raspberry Pi through a 40-pin universal input and output, which has multiple IC-based sensors that can be used for many different types of experiments, applications and games. The SenseHAT includes a Gyroscope, Accelerometer, Magnetometer , Barometer, Temperature sensor, Relative humidity sensor, 8x8 RGB LED matrix display and 5-way joystick.
- The Raspberry Pi camera offers 8MP resolution and features an image sensor that enables the board to capture 3280 x 2464 pixel static images. The camera supports 1080p30, 720p60 and 640x480p90 video, and links to the Raspberry Pi board through a dedicated CSi interface. The NoIR camera v2 has a No InfraRed (NoIR) filter on the lens which makes it the perfect option for infrared photography and taking pictures in lowlight environments.
element14 offers the full range of accessories for the Raspberry Pi, including exclusive boards and add-on modules to enable new and innovative projects. For more information visit www.element14.com/raspberrypi
element14 is the Development Distributor, supporting customers as they design, build and bring products to market. Whether makers or engineers, element14 provides the latest technology alongside support and inspiration from the element14 community.
Applicants should sign up for the content and submit their solution plan online by 27th October 2017. The best 50 solutions will be chosen to receive CNY 500 funding to develop their design for the opportunity to win a RMB 3000 shopping voucher*.
Completed designs should be submitted by uploading a detailed description of purpose and functionality, picture of the device or a video of how it works, by 4th January 2018. Winners will be announced by the end of February 2018.
To find out more and submit an entry visit http://www.eeboard.com/rpi3-contest/
* Awards (1 x the 1st prize, 3 x the 2nd prize, 5 x the 3rd prize, 10 x the honorable prize)
- 1st prize(1):RMB 3000 shopping voucher
- 2nd prize(3):RMB 1000 shopping voucher
- 3rd prize(5):RMB 500 shopping voucher
- honorable prize(10): 1 BBC micro:bit (RMB 100)
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/