element14 launches first all-in-one mangOH™ Green Open Hardware Platform
First in the market all-in-one Hardware, Software and Cloud-based solution for Industrial IoT applications from element14 and Sierra Wireless
element14 and Sierra Wireless today announce the launch of the mangOH™ Green Open Hardware IoT Platform and mangOH™ kit.
The mangOH™ Green Open Hardware IoT Platform allows developers to test and prototype ideas quickly and take IoT solutions to market within weeks. The industry’s first complete sensor-to-cloud platform, it provides an all-in-one hardware, software and cloud-based solution for industrial IoT applications. Ideal for data logging in a remote location, the mangOH™ Green Open Hardware IoT Platform is perfectly suited for remote monitoring systems, as well as multiple sensor, IoT, and cloud-based applications.
At the heart of the board are two industrial-grade CF3 connectors to enable the use of either an AirPrime HL Series module or an AirPrime WP Series applications processor module from Sierra Wireless. The AirPrime WP Series cellular modem provides the device-to-cloud architecture enabling IoT developers to build a Linux-based product on a single module.
Key features of its hardware, software and cloud services include:
Hardware
- Integrated ARM-based application processor with cellular modem and GPS
- Arduino and IoT Connector to add wireless, wired, and sensor technologies
- Battery enabled for low-power applications
Software
- Legato open source Linux platform with robust connectivity APIs for accessing cloud and mobile network services
Cloud Services
- Pre-integrated with the IoT Acceleration Platform from Sierra Wireless
The mangOH™ Green IoT Platform is also compatible with other open source initiatives to allow for easy and fast prototyping; these include NXP thread module, Linear Technology Dust Networks and Texas Instruments ZigBee, Wi-Fi and Bluetooth module.
We are delighted to work with Sierra Wireless to launch these first-to-market mangOH™ Green solutions. It is an innovative platform that will appeal to developers working on next-generation IoT designs.
The goal of the mangOH™ Green design is to remove the hardware complexity associated with prototyping IoT connected devices. We are excited that element14 has adopted the open source design and is manufacturing and selling the industrial-grade boards globally
The easiest way to get started is with the mangOH™ kit, which contains all of the components you need to get designing quickly. The kit contains a mangOH™ Green Base board, as well as a WP8548 module with Cortex A5 application processor, GNSS receiver and 3G modem, socket cover and release tool, two Breakout Board IoT Connectors, a power supply unit, antennas and USB cable.
Sierra Wireless is running a one hour webinar entitled ‘Using open source technologies to rapidly build secure IoT devices’ on 24th May 2016 at 5pm GMT. The event is sponsored by element14. To register please use the following link: https://webinar.techonline.com/2007?keycode=CAA1EC
These new kits are the latest in element14’s diverse variety of solutions ranging from starter kits to complete development boards, including the newest releases and exclusive bundles at its Design Center; www.element14.com/designcenter
For more details, downloads and to participate in discussions on mangOH Green go to: https://www.element14.com/community/docs/DOC-80845
The mangOH™ Green IoT Platform is available from Farnell element14 in Europe, Newark element14 and North America, and element14 in Asia.
Notes to editors
The mangOH development kit contains:
- a mangOH Green base board as well
- a WP8548 module with Cortex A5 application processor, GNSS receiver, and 3G modem
- CF3™ socket cover (to lock the module in the CF3 socket)
- CF3™ release tool (to remove the module from the CF3 socket)
- Breakout Board IoT Connector x 2 (sliders assembled)
- Power Supply Unit (PSU)
- Antennas
- USB cable
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/