End-to-end Sub-1 GHz kit for easy cloud connectivity exclusively from Farnell element14
Farnell element14, the Development Distributor, announces availability of the element14 development kit for the TI SimpleLink™ Sub-1 GHz Sensor to Cloud Linux® Gateway based on technology from Texas Instruments (TI). The kit provides an end-to-end tool to enable a Sub-1 GHz sensor network with an Internet of Things (IoT) gateway and cloud connectivity.
In the growing industrial IoT market, there is a need for connecting long-range low-power applications to the cloud. Developers face many challenges: they need a long-range low-power wireless protocol with regional regulatory compliance, and security is critical.
“Sub-1 GHz offers low-power and long-range wireless connectivity, but it doesn’t offer a native IP internet connectivity and is a fragmented band without a standard, making it complex to create a fully managed solution from the end nodes to the cloud.” says Simon Meadmore, Global Head of SEPO and SBC at Premier Farnell and Farnell element14: “Now, the element14 SimpleLink Sub-1GHz Sensor to Cloud Linux Industrial Gateway development kit, available exclusively from Farnell element14, allows developers to get to market faster with an out-of-the-box, end-to-end solution enabling an easy cloud connection for sending and receiving long-range sensor data while maintaining a robust link.”
The kit contains all the components needed to create a full sensor network, including a gateway design based on the BeagleBone® Black, the BeagleBone Wireless Connectivity Cape, and the TI SimpleLink dual-band CC1350 wireless MCU LaunchPad™ development kit acting as the MAC co-processor. The kit also includes an additional CC1350 wireless MCU LaunchPad kit acting as a long-range sensor node.
To provide a seamless out-of-the-box experience, the hardware comes pre-flashed with the SimpleLink CC13x0 software development kit (SDK), including the TI-15.4 stack for Sub-1 GHz star network connectivity and the TI Processor SDK Linux. It also provides a flexible IoT cloud interface giving the user the option to connect to a number of different cloud providers and addresses the challenges that developers face with building a long-range Sub-1 GHz network with cloud connectivity.
The SimpleLink sensor-to-cloud development kit is a robust, reliable, tool that is ready to be certified for regulatory compliance and has the necessary hardware and pre-integrated software to make it easy for users to being developing. The TI 15.4 stack provides a standards-based Sub-1 GHz network that is easy to use and alleviates the complexity of linking a user’s own Sub-1 GHz wireless network to the cloud.
The SimpleLink Sub-1 GHz Sensor to Cloud Linux kit is available to buy exclusively from Farnell element14 in Europe and Newark element14 in North America.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/