Energy infrastructure solutions from onsemi are now available from element14
onsemi leverages decades of experience in innovative, reliable and highly efficient next-gen power semiconductors to shorten development times while exceeding power density norms and reducing power loss

element14 announces the availability of the latest, highly optimised silicon carbide (SiC) EliteSiC products for energy infrastructure solutions from onsemi. These new devices meet next-generation performance requirements thanks to their reduced switching losses under real-world conditions when compared to their competitors.
The accelerating transition to decarbonisation is shifting demand toward the installation of more energy infrastructure systems featuring DC fast chargers (DCFC), solar inverters and battery energy storage systems (BESS).
Adopting silicon carbide-based power stages is critical in reducing power losses, increasing power density and reducing cooling costs. Selecting highly robust SiC power devices built with infrastructure-class reliability in mind is a key part of designing long lasting, rugged energy infrastructure systems. onsemi products can shorten development times while exceeding power density norms and reducing power loss.
Typical applications for onsemi EliteSiC devices, now available from element14, include UPS, DC/DC converters, boost inverters, solar inverters, electric vehicle charging stations and industrial power systems. These devices are Pb−free, halide free and RoHS compliant.
onsemi products now available from stock at element14 include:
- EliteSiC Power, Single N-Channel – with features including Typ. RDS(on)= 80 m, Ultra Low Gate Charge (Typ. QG(tot) = 56 nC), Low Effective Output Capacitance (Typ. Coss = 79 pF), TJ = 175°C and 100% Avalanche Tested
- EliteSiC MOSFET NXH006P120MNF2 - a power module containing a 6 m /1200 V SiC MOSFET half−bridge and a thermistor in an F2 package. Options include being supplied with or without pre−applied Thermal Interface Material (TIM) and solderable or press−fit pins.
Adrian Cotterill, Global Product Segment Leader, Transistors & WBG at element14, said: “This is a key addition to element14's portfolio that will ensure energy infrastructure systems are developed using the highest calibre, best-of-breed components for which onsemi is renowned. These new, highly optimised SiC products meet the latest performance requirements of energy infrastructure end applications.”
onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.
The new energy infrastructure solutions from onsemi are now available from stock at Farnell in EMEA, Newark in North America and element14 in APAC.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate