Leeds,
05
August
2020
|
09:30
Europe/Amsterdam

Farnell adds Mitsubishi Electric to enhance Industrial Automation range

A wide range of variable speed drives, PLCs and HMIs from Mitsubishi Electric are now available from Farnell for next day delivery across Europe.

FAR 546 - inline image

Farnell, the Development Distributor, has increased the depth and breadth of its industrial automation and control range with the introduction of some of the best-selling variable speed drives, Programmable Logic Controls (PLCs) and Human Machine Interfaces (HMIs) from Mitsubishi Electric, one of the world’s leading manufacturers in this key market.

Mitsubishi Electric’s automation and control products are suitable for a wide range of applications including smart manufacturing driven by the Industrial Internet of Things (IIoT) and Industry 4.0. System designers can easily integrate this electronic automation technology to develop new machinery and equipment much faster. Next day delivery across Europe will benefit engineers completing critical maintenance and repairs, allowing work to be carried out with reduced downtime and production losses.

Mitsubishi Electric’s variable speed drives, PLCs and HMIs complement Farnell’s existing industrial automation and process control portfolio, bringing higher productivity and quality to the factory floor.

 

Some of the most in-demand products by Mitsubishi Electric now available from Farnell include:

  • Variable Speed Drives: Mitsubishi Electric’s range of compact, flexible, versatile and cost-effective variable speed drives are designed for a service life of more than 10 years and incorporate many safety features.
    • The FR-D700 Frequency Inverter is a compact micro-drive solution offering simple, timesaving start up, increased energy savings with its Optimum Excitation Control (OEC) function, and a high overload capacity of 200 percent. Typical applications include feeder and conveyor drives, matching tools or gate and door drives.
    • The FR-E700 SC Frequency Inverter is an expandable compact drive solution with simple and fast installation. It is exceptionally user-friendly and has extensive communication options. This is an economical and highly versatile solution for a wide range of applications from textile machines to door and gate systems and material handling systems.
  • HMIs: Mitsubishi Electric’s HMIs boast advanced functionality, allowing users to control industrial automation devices using touch-sensitive graphic displays.
    • The GOT2000 Series features multi-touch gestures for intuitive operation. Objects may be enlarged, scrolled or flicked and critical operations can be controlled by designating two touch points. Models in the series are available with a range of screen sizes from 3.8 inch to 15 inch.
  • PLCs: Mitsubishi Electric is one of the world’s largest manufacturers of PLCs, renowned for offering exceptional reliability and performance.
    • The FX3 Series continues a design philosophy spanning more than a quarter of a century, with a customer base spread across the globe. The FX3S, FX3G and FX3U family of products provide an ideal solution for small to medium-sized control and positioning tasks requiring a combination of 10 to 384 inputs and outputs for industrial control and building services applications.
    • The FX5 Series with its completely redesigned high speed system bus and an extensive array of built-in features and enhanced security functions provides the new micro PLC with an outstanding level of performance. For standalone use to networked systems application the FX5 takes your business to the next level of industry.

Simon Meadmore, Global Head of IP&E at Farnell says: “Mitsubishi Electric is an innovator in factory automation technology, and this new agreement allows us to provide even more high quality, reliable products to our customers. The introduction of Mitsubishi Electric’s best-selling variable speed drives, PLCs and HMIs greatly enhance the depth and breadth of our industrial automation and process control portfolio, making Farnell a key supplier in Europe.”

Mitsubishi Electric is a large, well established company and one of the world’s leading names in the variable speed drives sector. The company is well known for producing quality, high-end products and has been at the forefront of Japan’s technical creativity and product innovation since 1921.

Farnell’s customers now have access to a greater range of market leading automation and control products with 24/5 technical support. This includes free online resources, data sheets, application notes, videos, and webinars on Farnell’s website.

The Mitsubishi Electric range of variable speed drives, PLCs and HMIs are available for fast shipping in Europe from Farnell in EMEA.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/