Farnell element14 announces availability of Weidmuller’s Klippon® Connect A-Series terminal blocks
The new A-Series uses innovative PUSH IN technology to deliver greater value add and productivity across the entire panel production
Farnell element14 has announced the availability of the Weidmuller Klippon Connect A-Series benefitting from simple handling, more space in the panel and time saving during installation.
The latest Klippon Connect A-Series applications products are designed for reoccurring panel applications such as 24V distribution or signal wiring for sensors and actuators. The PUSH IN technology provides greater flexibility and faster wiring times with up to 50% less time spent on installation.
Colour-coded connections simplify panel wiring and subsequent modifications and rewiring are possible due to the simple and practical functionality. The innovative, spring-based, direct insertion also guarantees vibration-resistant, gas-tight contacts even in challenging applications.
The new Klippon Connect A-Series terminal block portfolio consists of an application range and a universal range.
Weidmuller’s range of Klippon Connect blocks are available from Farnell element14 in Europe and element14 in Asia. For more information about Weidmuller’s product offerings, visit: http://uk.farnell.com/weidmuller.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/