Farnell element14 Introduces Vishay Capacitors for Energy Harvesting
Farnell element14 is launching the Vishay hybrid storage 196 HVC ENYCAP™ capacitors which are portable, compact and facilitate high-energy storage.
Priced from £13.39 with price breaks for higher volumes the capacitors have the industry’s highest energy density (13 Ws/g) as well as polarised storage capacitor with high capacitance (up to 90 F).
Ideal as a storage device for energy harvesting, the capacitors are an alternative to rechargeable backup batteries as they can hold 70% of their charge for as long as a month.
They support voltages ranging from 1.4V (single cell) to 2.8V / 4.2V / 5.6V / 7.0V / 8.4V (multiple cells) and are available as stacked through-hole (STH, radial), surface mount flat (SMF) and lay-flat configurations (LPC) with wire and connectors.
Their low profile (2.5 mm) means they are the right size for portable and compact designs.
Hybrid Storage 196 HVC ENYCAP™ Capacitors are part of Vishay’s famous Super 12 range and are available with next day delivery. For more information on the other products in the Super 12 range click here.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/