London,
18
April
2018
|
01:01
Europe/Amsterdam

Premier Farnell presents Aim TTi TGF3000 Series Dual Channel Arbitrary Function Generators

160 MHz and 80MHz models offer class-leading performance and unrivalled value for money

TGF3082

Premier Farnell, the Development Distributor, has added Aim TTi TGF3000 series Dual Channel Arbitrary Function Generators to its instrumentation range. The TGF3000 series is the latest arbitrary generator series from Aim-TTi offering class-leading performance and unrivalled value for money in 160 MHz and 80 MHz models.

The new TGF3000 series initially consists of two models, the TG3082 (dual channel, 80MHz, 14 bits / 400MS/s) and TG3162 (dual channel 160MHz, 16 bits / 800MS/s), two identical full performance channels that can operate as independent generators or in coupled or tracking modes. Precise channel to channel phase control with a resolution of 0.001o is provided. A wide range of built-in waveforms is included and custom arbitrary waveforms can be used at sample speeds up to 800MSa/s and replay rates up to 80MHz. PC based arbitrary waveform generation and editing software is provided. High resolution, low jitter pulses can be generated and the noise function provides wideband Gaussian noise at bandwidths up to 100MHz and crest factor of more than five. An extensive array of modulations is provided using internal and external sources. Gated, burst and sweep modes can use internal or external trigger sources. Remote control via USB and LXI compliant LAN (standard) can be supplemented by optional GPIB if required.

Key features include:

  • Frequency up to 160MHz, 15 digits or 1μHz resolution
  • Wideband noise generator | high resolution pulse generator
  • Arbitrary waveforms up to 16bits at 800MSa/s
  • Comprehensive internal/external digital and analog modulations
  • Two identical channels with phase control, coupling and tracking
  • USB and LXI compliant LAN interfaces, plus optional GPIB interface

The TGF3000 series is available to buy from Farnell element14 in Europe and element14 in Asia Pacific.

Boilerplate

About us

Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.

Premier Farnell is a business unit Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Premier Farnell sells direct to consumers through Forthings.io in the UK and IrelandSpainDenmarkFinland and Sweden, a network of resellers, and its CPC business in the UK.

For more information, visit the website at http://www.premierfarnell.com