Farnell element14 presents the new 6½ digit Keithley DMM6500 for exclusive pre-order
Digital Multimeter offers 5 inch touchscreen display, 1Msample/s digitizing as standard, 7M reading internal memory and increased sensitivity

Farnell element14 is offering customers in Europe the opportunity to pre-order the new 6½ digit Keithley DMM6500 for immediate shipment on 16 April 2018. The DMM6500 is a modern Bench/System digital multimeter (DMM) ideally suited for design engineers and production test engineers, delivering more measurement functionality, best-in-class measurement insight and a price that will not break the budget.
The DMM6500 is equipped with all the measurement functions you would expect in a bench multimeter, eliminating the need to buy additional measurement capabilities. It has 15 measurement functions including capacitance, temperature (RTD, thermistor and thermocouple), diode test with variable current sources, and up to 1 MS/sec digitizing. The digitizing function can be used for voltage or current and is especially useful in capturing transient anomalies or to help profile power events such as the operating states of today’s battery operated devices. Current and voltage can be digitized with a programmable 1 MS/sec 16-bit digitizer, making it possible to acquire waveforms without the need for a separate instrument.
The most recognizable feature of the DMM6500 is the large 5-inch capacitive touch display that makes it easy to observe, interact with and explore measurements with “pinch and zoom” simplicity. Beyond its display technology, the DMM6500 superior analogue measurement performance delivers 25 PPM basic DCV accuracy for one year and 30 PPM for two years, allowing users to extend calibration cycles.
Key benefits include:
- More measurement functions and wider measurement ranges (including 10 µA to 10 A and 1 mΩ to 100 MΩ) with more sensitivity to maximize the utility of the DMM and to enable measurements on new, low power components and products
- 1Msample/s digitizing to capture complex waveforms and transients
- A 5 inch (12.7cm) multi-touch capacitive touchscreen display with readily accessible swipe screens and minimized menu depth and to enable fast, in-depth data analysis. Graphing, pinch and zoom, cursors, and statistics enable design engineers to get greater insight into measurement trends and waveform characteristics
- Fastest integrating measurements to reduce test time in automated systems
- Test script processing (TSP) to reduce time-consuming communications with a PC and to customize measurements for specific applications
- Optional scan cards to expand the number of measurements that can be taken with a single DMM
- Emulation of the Keithley 2000 DMM and to permit upgrading hardware while avoiding the need to write new test code
- Large internal memory - store up to 7 million readings, additional USB host port for storing readings, instrument configurations and screen images
- 2-year specifications to reduce the cost of ownership
- 3-year warranty
The Keithley DMM6500 is available for pre-order from Farnell element14 in Europe.
About us
Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Premier Farnell is a business unit Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Premier Farnell sells direct to consumers through Forthings.io in the UK and Ireland, Spain, Denmark, Finland and Sweden, a network of resellers, and its CPC business in the UK.
For more information, visit the website at http://www.premierfarnell.com