Farnell shipping new Bluetooth® 5.0 Low Energy module from Panasonic
Pan1780 low energy Bluetooth module with -95dBm sensitivity ideal for IIoT devices and Smart Home applications
Farnell, the Development Distributor, is now shipping the PAN1780 Bluetooth® Low Energy Module from Panasonic, a Bluetooth® 5.0 Low Energy (LE) module based on the Nordic nRF52840 single chip controller. Farnell are also the only high service distributor to hold this module in stock in Europe, with orders despatched the same day.
The compact module, which measures just 15.6 mm x 8.7 mm x 2 mm, uses Bluetooth 5.0 with the qualified Bluetooth® mesh profile stack, and is ideal for IoT devices within smart city infrastructure, industrial mesh networks or robotics within Industry 4.0 environments:
- The Cortex® M4F processor, 256 kB RAM and build-in 1 MB flash memory eliminate the need for an external processor saving complexity, space, and cost
- Ultra-low current consumption makes the module ideal for battery powered devices
- Output power of up to 8 dBm and the high sensitivity of the nRF52840 in combination with the LE coded PHY support applications where a long range is required
- A rich set of security features from the ARM TrustZone CryptoCell 310 security subsystem enable secure device operation ideal for smart health and secure medical peripherals, or edge computing.
The Bluetooth® 5.0 enables a higher symbol rate of 2 Mbps via the high-speed LE 2M PHY with significantly longer range possible using the LE coded PHY at 500 kb/s or 125 kb/s. In addition, new LE advertising extensions allow for much larger amounts of data to be broadcasted in connectionless scenarios. The PAN1780 also supports Type 2 Near Field Communication (NFC-A) for use in simplified pairing and payment solutions (external antenna required).
The module has an operating temperature range of -40°C up to 85°C and also benefits from a built-in temperature sensor.
The Panasonic PAN1780 Bluetooth® Low Energy Module is available from Farnell in Europe, element14 in APAC and Newark in North America.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate