MATRIX Voice from MATRIX Labs available from Premier Farnell
Platform enables users to integrate custom voice and hardware-accelerated machine learning technology right onto the silicon

Premier Farnell, the Development Distributor, is shipping the MATRIX Voice from MATRIX Labs, available from Farnell element14 in Europe, element14 in Asia Pacific and Newark element14 in North America. The MATRIX Voice enables users, makers, and developers to create IoT applications based on sound driven behaviours, quickly and efficiently.
As the Internet of Things continues to expand, the prospect of developing unique IoT solutions should excite makers, engineers, and hobbyists. However, the process of successfully integrating artificial intelligence, hardware, and software in order to create a viable solution can be both expensive and time-consuming. The MATRIX Voice aims to lower the barriers to entry for the creation and deployment of IoT voice applications.
Powered by a Raspberry Pi computer or used as a standalone device with the ESP32, the MATRIX Voice specifically targets the development of voice recognition and detection projects, allowing users to utilise existing platforms such as Google Assistant or Amazon Alexa, or any other voice recognition API. The platform gives users the ability to integrate custom voice and hardware-accelerated machine learning easily into their applications. Beamforming, noise cancellation, far-field speech recognition, and de-reverberation capabilities ensure high quality performance for all voice applications.
Hari Kalyanaraman, Global Head of Emerging Businesses for Premier Farnell said: “As the Development Distributor, we strive to provide our customers with the very latest technology to help them as they bring their products to market. Platforms such as the MATRIX Voice give makers and entrepreneurs a real head start, enabling them to shrink their product development cycle and accelerate time to market.”
Rodolfo Saccoman, CEO and Co-Founder of MATRIX Labs says : “At MATRIX Labs, we aim to democratize the intersection between hardware, AI, and software. We have created hardware and accompanying operating systems to enable solutions, creations, and new companies to succeed. Instead of a company trying to build their own board, they can package our MATRIX Voice, manufacture any kind of casing, and then take their product to market- fast."
The MATRIX Voice board, at 3.14 inches in diameter, features a Xilinx Spartan-6 FPGA, 64 Mbit SDRAM, a 8 MEMS microphone array, and 18 LEDs among other features including an optional Wi-Fi attachment. 64 GPIO expansion pins—40 of which are used to connect to a Raspberry Pi—allow for additional customization.
MATRIX Voice is available from Farnell element14 in Europe, element14 in Asia Pacific and Newark element14 in North America.
About us
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/