New NXP V3 LPC Xpresso development boards from element14 for faster evaluation-to-production
More choice and flexibility to easily add more functions to projects via compatible shields
element14 has announced the addition of three new NXP development boards in the LPC Xpresso family to its extensive portfolio of technology products, which includes the biggest range of development kits available globally from one single source.
These new LPC Xpresso V3 boards are part of an established and popular toolchain featuring the power of LPC microcontrollers based on ARMs Cortex-M cores. The boards are able to work with most existing LPC Xpresso accessories and Arduino compatible shields to enhance functional capabilities, offering more versatility for applications in motor control, power management, white goods, RFID readers, embedded audio applications, industrial automation, and e-metering.
David Shen, Group Chief Technology Officer at Premier Farnell said, “We are excited to work with NXP to add these new Xpresso V3 boards to the highly popular LPC Xpresso ecosystem. With the built-in debug probe, PMOD and Arduino connectors as well as an additional row of expansion port pins, these boards offer a rich hardware and software experience for rapid prototyping of products based on the LPC8000 and LPC4300 dual-core microcontrollers.”
LPC Xpresso 18S37 - ARM Cortex MCU development board offers evaluation and prototyping opportunities for the LPC1800 LPC MCU family; it features an ARM Cortex-M3 core running up to 180MHz
Both LPC Xpresso 4337 and 43S37 ARM Cortex MCU development boards offer evaluation and prototyping opportunities for the LPC4300 LPC MCU family; it features dual ARM cores (M4F and M0+) running up to 208MHz
Both the 18S37 and 43S37 include an AES hardware encryption engine for protecting data communications and application code in required in multiple applications including IoT.
The LPC General Purpose Shield Board works with V2, V3, and MAX LPCXpresso MCU development boards to provide easy access to several commonly used peripherals like LCD dot matrix display, user LEDs and 5 position joystick, inertial and temperature sensors and more. Join the discussion at http://www.element14.com/community/docs/DOC-74446
The NXP LPC Xpresso boards are available from Farnell element14 in Europe (priced from £12.35), Newark element14 in North America (priced from $25.00), and element14 in Asia (priced from S$35.18); details are available at http://www.element14.com/community/docs/DOC-74693
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/