Chicago,
27
June
2019
|
16:00
Europe/Amsterdam

Newark Adds Micro-B Connectors from Amphenol Industrial Operations

Amphenol Micro B connectors_large

Newark, the Development Distributor, continues to offer its community of designers with the varied connector options they need to advance their designs with the addition of the Micro-Bayonet (Micro-B) connectors from Amphenol Industrial Operations. This product line provides an affordable alternative to connectors used in industrial markets requiring high signal counts and small packages.

The Micro-B series offers lightweight, high performance connectors with a small footprint that utilize a robust triple bayonet coupling, providing quick and positive locking. The Micro-B series is ideal for industrial designers seeking high electrical performance at a low price. The new circular connector series is designed for industrial applications such as Telecommunications, HEV, Robotics/Factory Automation, Industrial Instrumentation, Security, and Test Equipment where electrical performance must be met with affordability.

Micro-B meets the requirements of today’s electrical equipment by delivering excellent shell-to-shell electrical bonding for EMI required in rugged connectors. The compact Micro-B features high density insert patterns with size 22D contacts allowing for more circuits to be connected and a simplified termination process with tape and reel contacts. It also offers tool-less and fast mating for ease of use in the field.

Further technical information:

  • RoHS-compliant circular connector series
  • Various mounting options available, including in-line and 2-hole flange mount configurations
  • Operating temperature of -40°C to +125°C, a dielectric withstanding voltage of 500 VRMS and a current rating of up to 3 Amps per contact. It is durable up to 500 mating cycles
  • With Gray ZnNi plating, Micro-B can withstand up to 500 hours salt spray without corrosion detrimental to its operation

Amphenol Industrial Operations is a global leader in interconnect systems for harsh environment applications.

Micro-B connectors from Amphenol Industrial Operations are available from Newark.

Boilerplate

About us

Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.

Premier Farnell is a business unit of Avnet (Nasdaq: AVT). Premier Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Premier Farnell sells direct to consumers through a network of resellers, and its CPC business in the UK.

For more information, visit the website at http://www.premierfarnell.com