Newark element14 exclusively presents a new way to observe the micro-world – wirelessly
Exclusive distribution agreement for the sale of Visio-tek branded products
Newark element14 has signed a one-year exclusive distribution agreement for the sale of Visio-tekTM branded products. Visio-tekTM is a line of versatile and portable, digital microscopes that utilize both Wi-Fi and USB transmission alongside a 1.3mpx camera and up to 600x magnification.
Visio-tekTM digital microscopes enable real time digital inspection and multi-sharing, wherever you are, through the convenience of viewing images through one or multiple mobile devices. The range includes six microscopes and four stands, suited to limitless applications, from industrial and electronic inspection and quality control to research and scientific analysis, education and forensics.
Options include:
- White LED’s/Lights: The standard model suitable for multipurpose applications which allows you to see the natural and visible spectrum of light.
- White LED’s/Lights + Polarizer: Polarizing the light increases and maximizes vision quality.
- White LED’s + UV LED’s + IR LED’s: For scientific and medical applications where UV or IR light is required.
- 500-600x: The highest power model for applications requiring the greatest magnification.
- White LED’s + UV LED’s: UV light is essential for seeing elements that are made with chemical structures which react to UV.
- White LED’s, Long Distance: Designed for applications where increased clearance is beneficial while working under magnification.
Visio-tekTM Digital Microscopes can be connected to iOS and Android smartphones or tablets via the Visio-tek App, as well as through a Wi-Fi/USB connection to Windows and Mac computers or laptops, enabling you to capture pictures, shoot video and take measurements either on the go or in the lab.
The range of Visio-tekTM digital microscopes and stands is available exclusively from Newark element14. To find out more visit http://www.newark.com/visio-tek or call 1-800-463-9275.
Notes to Editors
Additional images are available below.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/