Premier Farnell announces availability of Microchip SAM L10 and SAM L11 Evaluation Kits suitable for a range of IoT applications
Microchip SAM L Family of Microcontrollers deliver Ultra-Low-Power, Integrated Security and Superior Touch Control
Premier Farnell, the Development Distributor, has announced the availability of the Microchip SAM L10 and SAM L11 Xplained Pro Evaluation Kits and associated MCUs. The new devices are the industry’s lowest-power 32-bit MCUs as well as the first to offer chip-level security and Arm® TrustZone® Technology.
The SAM L10 is the industry’s lowest power MCU in this class and allows users to develop secured applications without the battery constraints of less power-efficient MCUs. Its ultra-low power consumption makes it suitable for a range of IoT applications in areas such as wearable devices, gaming controls, energy harvesting, smart pens and low-power industrial sensor nodes.
The SAM L11 additionally features integrated hardware security which allows users to take advantage of the increased security needed by applications such as IoT nodes, remote keypads and authentication systems for smart cities and home automation; industrial automation or medical devices.
“With the increasing growth of IoT end points and the resultant increased frequency of security breaches, designers are looking for MCUs that can help reduce power consumption while adding robust security”, says Simon Meadmore, Global Head of Semiconductors, Premier Farnell: “As the Development Distributer we seek out devices to address design challenges for our customers as they bring their products to market. The SAM L10 and SAM L11 MCU family takes an innovative approach to solving these challenges by integrating a wide variety of peripherals, including security features, into the industry’s lowest power MCU in its class. This allows users to develop secured applications without the battery constraints of less power-efficient MCUs.”
The new MCUs run at 32 MHz with memory configuration of up to 64 KB Flash and 16 KB SRAM. In addition to their ultra-low power consumption, they incorporate an enhanced Peripheral Touch Controller and advanced analogue features. Both devices are available in 24- and 32-pin package options.
In addition to being the industry’s lowest power MCUs in their class with an EEMBC certified ULPMark of 405, the SAM L10 and SAM L11 are built with picoPower® technology and provide flexible power saving modes. They are supported with power debugging and data visualiser tools to monitor and analyse power consumption in real time, helping developers to rapidly optimise their system designs for lower power consumption with significant improvements in battery life.
Designer of appliances, fitness trackers, automotive door handles, key pads or remote controls will benefit from the enhanced Peripheral Touch Controller (PTC), which provides best-in-class water tolerance and high noise immunity. Superior capacitive touch interfaces become easy to incorporate in users’ applications. The interface is four times faster than previous generations of PTCs and provides highly-responsive and accurate touch sensing. It is supported by the QTouch Configurator and QTouch® Modular Library, which make it simple to add elegant touch interfaces to designers’ applications.
The chip-level security incorporated into SAM L11 MCUs is based on ARM® TrustZone® technology to help protect against both physical and remote attacks plus a comprehensive security solution framework to simplify the implementation of security. IoT nodes driven by a SAM L11 provide strong resistance to remote software attacks, thereby increasing the reliability and avoiding any downtime of the critical functions of the nodes. The chip-level tamper resistance will help protect from cloning and intellectual property theft.
Both MCUs are available as development kits: the SAM L10 and SAM L11 Xplained Pro Evaluation Kits. These are fully supported with security, low-power and touch demos to accelerate development and help customers get their designs to market faster.
The Microchip SAM L10 and SAM L11 evaluation kits and associated MCUs are available from Farnell element14 in Europe, Newark element14 in North America and element14 in Asia Pacific.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/