Premier Farnell launches GraspIO Cloudio - a Raspberry Pi expansion board with a mobile platform for end to end IoT development and deployment
Expansion board enables Prototyping and Play with Drag and Drop programming mobile app, IoT Cloud, Voice Assistant Capabilities, IFTTT integration, Sensor monitoring, and more
Premier Farnell, the Development Distributor, announces the launch of GraspIO Cloudio - a Raspberry Pi add-on board with Drag and Drop programming interface on iPhone, iPad, Android. Among other features, it incorporates Voice Assistant Capabilities, IFTTT (“If This Then That”) Integration, IoT Cloud Service, Sensor Monitor and Dashboard, Custom Notifications with Image and Video and One Tap Multi-Board Upload.
“The versatility of GraspIO Cloudio along with its ease of use will make it popular with makers and innovators in a wide range of application environments. Cloudio, when combined with a Raspberry Pi, is a Full Stack IoT platform meaning that you can programme IoT devices simply and quickly with drag and drop programming on a mobile app,” says Steve Carr, Global Head of Marketing at Premier Farnell. “The combination of built-in hardware facilities and access to innovative application software will make Cloudio a valuable addition to the range of tools available to developers of projects involving voice, motion, imaging and cloud interaction.”
Cloudio unlocks physical computing applications with Raspberry Pi through a feature-packed board that includes a 0.96-inch OLED display, IR sensor, light sensor, temperature sensor, tactile switch, three ADC ports, a mini servomotor port for external sensors, three digital output ports, an RGB LED, and a buzzer.
Potential applications for the Cloudio include:
-
Voice Control: Users can create their own voice assistants using the inbuilt speech recognition feature to control Cloudio from a smartphone. Customised voice commands can be set to control lights, fans, switches, locks, and more, from anywhere.
-
Speech Output: Projects can be made to “talk” with the easy-to-use in-application “Speak” block and the Raspberry Pi’s own headphone jack. Users can create real-time speech notifications and custom messages, or play recorded audio from the board.
-
IFTTT Integration: IFTTT meets physical computing with Cloudio. Users can create simple applets that use Cloudio’s features as both triggers and actions for a new connected experience. One connection, countless possibilities.
-
Sensor Monitor and Dashboard: Using Cloudio’s on-board or external sensors, it can be deployed as an edge device to design intelligent and responsive sensor monitoring projects. Real-time sensor graphs can be viewed on a mobile device and data can be exported for IoT analytics.
-
Camera and Custom Notifications: A Raspberry Pi or USB camera can be interfaced effortlessly with the in-application camera block to capture images and videos or to create GIFs and time-lapse videos. Users can keep an eye on their projects by adding email, image, and video notifications.
Cloudio is designed and developed by Grasp IO Innovations and exclusively manufactured and distributed by Farnell element14. GraspIO aims to make the world of IoT and Robotics less technical and more practical for learning, prototyping, and play. A video showing potential Cloudio projects can be seen here.
GraspIO Cloudio is available to buy from Farnell element14 in Europe, element14 in APAC and Newark element14 in North America.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/