Premier Farnell launches The Things Network, Gateway, Uno and Node for the easy development of low cost, low power, long distance IoT networks
Premier Farnell, the Development Distributor, is pleased to announce the availability of a new range of LoRaWAN™ products from The Things Network. The Things Gateway, The Things Uno and The Things Node, enable users to create LoRaWAN internet of things networks quickly and easily. Using The Things Network Gateway you can setup a LoRaWAN network in just 5 minutes – you can then use The Things Node to create a LoRaWAN prototype in one hour and develop a LoRaWAN proof of concept within a day using The Things Uno. The three products are available to buy from Newark element14 in North America and Farnell element14 in Europe.
The Things Network, a collaborative IoT data network, made its successful debut by covering the city of Amsterdam with LoRaWAN coverage – a protocol for high capacity, long range and low power for the Internet of Things. There are now 500 developer communities in 94 countries vouching for this user operated network.
The products include:
-
The Things Gateway – The LoRaWAN base station enables ‘things’ to connect to the internet. With an easy to use gateway users can create the most substantial aspect of the IoT data network. Not only does The Gateway, provide up to 5km/ 3 miles radius of network coverage but it can also connect up to 10,000 devices.
-
The Things Uno – The Things Uno is a useful board to realise IoT use cases. The Uno gives IoT projects long range connectivity (up to 10km) and comes with an added Microchip LoRaWAN module and embedded antenna. It is fully compatible with the Arduino IDE and existing shields.
-
The Things Node – The Node is the perfect LoRaWAN device to start prototyping your ideas without having to deal with breadboards, wires and sensors. The Things Node is based on the SparkFun Pro Micro and has an added Microchip LoRaWAN module along with an embedded antenna. It contains a temperature sensor, digital accelerometer, a light sensor, button, and RGB LED.
The three products will allow users to get started with LoRaWAN in the fastest way possible.
With the support of a global community and technical resources, as well as easy cloud integration with popular IoT platforms, users can set-up their own LoRaWAN network in five minutes or create a LoRaWAN sensor prototype in just 60 minutes.
With the development of user- owned networks, providing low power and long-distance connectivity, The Things Network range of products enable use cases which have never been possible before. Applications ranging from smart parking and vehicle management to air quality and pollution monitoring can now be easily rolled out, without the need for extensive hardware or software skills.
Steve Carr, Global Head of Marketing for Premier Farnell says: “As the Development Distributor we seek out the latest technology products that enable our customers to develop solutions quickly and easily. We are delighted to be working in partnership with The Things Network, for the manufacture and distribution of these products. The application of LoRaWAN to deliver long range, low power networks creates huge opportunities for innovation and truly democratizes the Internet of Things.”
Wienke Giezeman, Initiator of The Things Network, says: “After our success on Kickstarter we are very happy to be able to say that the products are now available in the North America and Europe. Our mission is to make LoRaWAN easy for developers. As a developer you want to invest your time in making your IoT application and not in reinventing the wheel. These LoRaWAN “out-of-the-box” network and prototyping boards will get developers started in no-time.”
To find out more about LoRaWAN please visit http://uk.farnell.com/lorawan-101
The Things Network products are available to buy from Newark element14 in North America and Farnell element14 in Europe.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/