Premier Farnell Now Stocking KEMET KC-LINK Capacitors for Fast Switching Wide Bandgap Semiconductor Applications
Typical applications include electric autonomous vehicles and power converting

Premier Farnell, The Development Distributor, now stocks KC-LINK Surface Mount Capacitors from KEMET, manufacturers of advanced capacitors and components.
KEMET’s KC-LINK surface mount capacitors are designed to meet the growing demand for fast switching semiconductors that operate at a higher voltage, temperature and frequency. With an operating temperature of up to 150°C, these capacitors can be mounted close to fast switching semiconductors at very high power density applications, which require minimal cooling.
KEMET utilizes a proprietary C0G/NPO base metal electrode dielectric system, making the capacitors well suited for power converters, inverters, snubbers and resonators, where high efficiency is a primary concern. With extremely low effective series resistance (ESR) and very low thermal resistance, KC-LINK capacitors can operate at very high ripple currents with no change in capacitance versus DC voltage and negligible change in capacitance versus temperature.
The KC-Link C0G dielectric technology also provides high mechanical robustness compared to other dielectric technologies, allowing the capacitor to be mounted without the use of lead frames. This provides extremely low effective series inductance (ESL) that increases the operating frequency range, allowing further miniaturization.
Other benefits include an operating temperature range of −55°C to +150°C, high frequency operation (>10 MHz), no piezoelectric noise and the capacitors are also RoHS Pb-free. Automotive grade devices are also available to meet the demanding Automotive Electronics Council’s AEC–Q200 qualification requirements.
Typical applications include:
-
Wide bandgap (WBG), silicon carbide (SiC) and gallium nitride (GaN) systems
-
Hybrid electrical vehicles (drive systems, charging)
-
Photovoltaic systems
-
Power conversion
-
Inverters
-
DC link
-
LLC resonators
KEMET KC-LINK surface mount capacitors are now available to buy from Farnell element14 in Europe and Newark element14 in North America.
About us
Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Premier Farnell is a business unit Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Premier Farnell sells direct to consumers through Forthings.io in the UK and Ireland, Spain, Denmark, Finland and Sweden, a network of resellers, and its CPC business in the UK.
For more information, visit the website at http://www.premierfarnell.com