London,
27
March
2018
|
01:00
Europe/Amsterdam

Premier Farnell now stocking Rohde & Schwarz® RTC1000 and RTM3000 Oscilloscopes

New range of Oscilloscopes provides state-of-the-art and high performance technology, for embedded developers, service technicians and educators

RTM%20angle

Premier Farnell, the Development Distributor, is now stocking two new oscilloscopes from Rohde & Schwarz®, providing value and performance for all budgets.

The Rohde & Schwarz® RTC1000 oscilloscope is ideal for a broad range of users from embedded developers and service technicians to educators, who are looking for professional level functionality at a great price. State-of-the-art, high-performance technology, alongside an extremely silent design for better results, enables this multi-functional X-in-one product to meet even the demanding requirements of today’s customers. The oscilloscope also includes a wide range of upgrade options, providing true investment protection for the future.

R&S® RTC1000 key features include:

  • Up to 2 Gsample sampling rate and 2 Msample memory depth
  • Low-noise measurement due to state-of-the-art A/D converters
  • Versatile measurement functions and fast results
  • Wide selection of automatic measurement functions including:
    • QuickView: Key results at the press of a button
    • Mask test: easy creation of a new mask with just a few keystrokes
    • FFT: An easy way to analyse the signal spectrum
  • A 10-in-1 oscilloscope including: Oscilloscope, logic analyser, protocol analyser, waveform and pattern generator, digital voltmeter, component tester, frequency analysis mode and mask test mode

The Rohde & Schwarz® RTM3000 is a product that satisfies the all-important rule of investment protection at a very attractive price. More than just an oscilloscope, it includes a logic analyser, protocol analyser, waveform and pattern generator, digital voltmeter and dedicated operating modes for frequency analysis, mask tests and long data acquisitions. Users can quickly and efficiently debug all types of electronic systems.

Designed as an everyday problem solving tool, the R&S® RTM3000 combines the power of ten (10-bit ADC, 10 times the memory of the R&S® RTC1000 and a 10.1" touchscreen) along with a Rohde & Schwarz probe interface, which can be used with all Rohde & Schwarz® probes.

R&S® RTM3000 key features include:

  • Large 10.1” capacitive touchscreen - the largest capacitive display (10.1") with the highest resolution (1280 × 800 pixel) in its class. Users can simply touch the screen to quickly navigate onto pop-up menus and use gesturing to easily scale, zoom and move a waveform, just like using a smartphone.

  • Rohde & Schwarz designed 10-bit ADC - yielding up to a fourfold improvement over conventional 8-bit A/D converters. Users will get sharper waveforms with more signal details.

  • 40 MSample (all channels) and 80 MSample (interleaved) acquisition memory depth - 40 Msample memory depth is available on each channel if all channels are active. When interleaved, 80 Msample is available to capture longer signal sequences for more analysis results.

  • 10 second boot time

James McGregor, Head of Test and Tools, Premier Farnell said: “The Rohde & Schwarz® RTC1000 and RTM3000 oscilloscopes offer professional level capabilities at budgets to meet all needs, from budget conscious developers and educators, to professional design engineers looking for high performing multifunctional tools with value and future-proofing built in”.

The Rohde & Schwarz® RTC1000 and RTM3000 are available from Farnell element14 in Europe, Newark element14 in North America and element14 in Asia Pacific.

Boilerplate

About us

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/