London,
20
February
2018
|
01:00
Europe/Amsterdam

Premier Farnell now stocking the Aim TTi LDH400P Electronic Load

CAT II rated for High Voltage load testing

2800960-40

Premier Farnell, The Development Distributor, is now stocking the LDH400P Electronic Load from Aim TTi, manufacturers of advanced electronic test and measurement equipment and laboratory power supplies, specifically for electronic design engineers.

The LD series features electronic loads which are suitable for testing and characterising a wide variety of DC power sources. They can be used to investigate the behaviour of many different types of power source, such as: PFCs, batteries, solar cells and electronic power supply units. Wide voltage/current range, multiple operating modes and built-in transient generators also give users versatility to offer test solutions from the design laboratory through to the component test area.

As LDH400P load inputs are rated to CAT II (300V), direct testing of PFCs and main connected power supplies can be done without the need for an isolation transformer, saving bench space and cost.

Key features include:

  • Versatile solutions for direct testing of DC power sources and PFCs

  • Constant current, resistance, conductance and power modes

  • Wide voltage and current range, 10 to 500V and 0 to 16A

  • 400 watts continuous dissipation at 28°C (360W at 40°C)

  • High resolution and accuracy for level setting

  • Built-in transient generator with variable slew

  • Current monitor output for waveform viewing

  • Variable drop-out voltage for battery testing

  • High resolution backlit graphic LCD with soft key control

  • Analogue remote control of levels and TTL control of on/off and transient switching

  • Front and rear input terminals

  • Load inputs rated to CAT II (300V)

  • Full bus control via USB, RS232, GPIB and LXI compliant LAN interfaces

The Aim TTi LDH400P Electronic Load is now available to buy from Farnell element14 in Europe, Newark element14 in North America, and element14 in Asia Pacific.

 

Boilerplate

About us

Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.

Premier Farnell is a business unit Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Premier Farnell sells direct to consumers through Forthings.io in the UK and IrelandSpainDenmarkFinland and Sweden, a network of resellers, and its CPC business in the UK.

For more information, visit the website at http://www.premierfarnell.com