Premier Farnell now stocking the EA Elektro Automatik EA-EL 3000 B DC Electronic load Series for automated testing

Premier Farnell, The Development Distributor, is now stocking the EA Elektro Automatik EL 3000 B Series for automated testing in workshops, laboratories, education, R&D and industry.
This series is an ideal benchtop tool for low-power component- and device testing, providing accurate and reproducible test data. The versatile control software EA Power Control (available as free- and pay-ware) allows to run semi-automated test routines.
The unit, which has a significantly improved reaction time of analog and digital controls over the previous model, also benefits from:
-
400W, 0-80V, 0-200V, 0-500V DC, 0-10A up to 0-60A
-
Coloured TFT Display, with integrated comfortable function generator as well a battery test and (PV) MPP-tracking simulation
-
High-performance, micro-processor based control unit
-
16 Bit ADC/DACs for a high resolution
-
Voltage accuracy of 0.1% and current accuracy of 0.2%
-
Highly isolated structure resulting in lower sensitivity todisturbances during operation
-
Active damping in the DC-input circuit significantly reducing oscillations
-
Optimized thermal management eliminating a sudden stop upon an over-temperature condition
-
Input-filter protection circuit, preventing damage from DC voltage may contain a high-frequency AC part
-
Plug’n play slot to retrofit interface options eg USB
Typical applications include dynamic load testing and aging simulation of small DC sources, load testing/discharging of all types of energy storage devices and testing of semiconductors, passive and active electronic components.
The EA Elektro Automatik EL 3000 B Series is now available to buy from Farnell element14 in Europe, and element14 in Asia Pacific.
About us
Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Premier Farnell is a business unit of Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere.
For more information, visit the website at http://www.premierfarnell.com