London,
16
March
2017
|
10:00
Europe/Amsterdam

Premier Farnell shipping Infineon shields for Arduino

400x500shieldbtf3050tetobo1.jpg

Premier Farnell, The Development Distributor, is now shipping the Infineon 24V Protected Switch Shield and the Low-Side Switch Shield both for Arduino.

The 24V Protected Switch Shield is a power switch evaluation board compatible with Arduino microcontroller boards and Infineon’s XMC™ microcontroller kits using the Arduino form factor. It provides fast and inexpensive prototyping of 24V load driving, making it ideal for use in applications such as truck bulbs, car bulbs, valves, motors, relays, capacitors, and LEDs.

The shield is equipped with three PROtected high-side power MOSFETs out of the PROFET™+ 24V family, offering five 24 V channels in total. The power switches are controlled via the INx (input) pins. The PROFET™+ 24V devices also provide a sense current at the IS pin, which can be enabled via the DEN (Diagnosis ENable) pin. For the two channel devices the sensed channel is selected via the DSEL (Diagnosis SELect) pin. For each device the sense signal (IS) is connected to an own ADC channel of the microcontroller.

Infineon’s PROFET™+ 24V protected high-side switches drive resistive, capacitive and inductive loads with either a PWM of up to 400Hz or DC. It includes a driver circuit with logic level inputs, as well as load diagnosis with current sense capability and over temperature shut down with latch behaviour providing protection against over temperature, over current and ESD. This shield can handle 8 ~ 36V nominal input voltage (max. 5 ~ 48V) and a nominal current up to 5A per channel restricted due to PCB (nominal current: 7 A).

The Low-Side Switch Shield from Infineon consists of three BTF3050TE low-side switches of the HITFET™+ family providing three independent power channels that can be controlled via the input pins. The shield is compatible with microcontroller boards using the Arduino form factor and supports fast and easy prototyping of applications with BTF3050TE. With a nominal load current of 3A the BTF3050TE is able to drive resistive, inductive and capacitive loads. Furthermore the smart low-side switch provides diagnosis and protection features against items such as over temperature shut down with auto restart behaviour and double current limitation for inrush current. It also includes a latched and stable fault signal which is independent of the input pin. The Low-Side Switch Shield has a driver circuit with logic level inputs and can be driven with PWM up to 14 kHz (10% duty cycle) and with a 50 mΩ single channel switch, nominal battery voltage range from 8 ~ 18V and a nominal load current of 3A (typ.) DC this switch provides a fast and inexpensive way of prototyping for a wide range of applications.

The shields are available from Farnell element14 in Europe, Newark element14 in North America and element14 in APAC. Please visit the element14 Community for more information on the Infineon 24V Protected Switch Shield and the Infineon Low-Side Switch Shield.

Boilerplate

About us

Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.

Premier Farnell focuses its offering around four core customer journeys:

  • Education to Maker – Premier Farnell is an official manufacturer of two of the most popular Maker Boards, Raspberry Pi and Beaglebone Black, and exclusive manufacturer of educational programming boards such as the BBC micro:bit and Codebug. Customers are supported through element14.com, the largest online engineering and maker community, also providing support to educators and parents through its new STEM space.

  • Research and Design Services - Premier Farnell is the No.1 for Development Kits, having worked with the world’s leading Semiconductor companies to design and manufacture their latest development boards in house. A deep understanding and design knowledge of the latest Semiconductor Devices available also supports Premier Farnell’s broader design assistance offering, providing a similar service to customers of all sizes who are seeking additional engineering support.

  • Design through to Production – Premier Farnell provides an entire solution for design to manufacturing customers, with the broadest range of Semiconductor and Passive inventory available, a world class line card, same day despatch, a strong board level Interconnect proposition and growing Electromechanical proposition. In addition, it has the technical support capabilities to meet all customers’ needs, from simple cross-reference to complex design.

  • Bench to Board – Premier Farnell offers one of the industry’s broadest ranges of Test & Measurement equipment and a leading line card for all Tool & Production supplies supporting customers from the testing of initial designs to delivering essential maintenance activity to keep their operations running.

Premier Farnell is a business unit of Avnet Electronics Marketing, the components operating group of Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere.

Key facts:

  • Operations in 38 countries and 43 local language transactional websites

  • More than 3,500 leading suppliers

  • More than 650,000 products stocked with access to over four million more on demand

  • More than 440,000 members of the element14 community

  • Leaders in providing information on REACH, Conflict Minerals and EU RoHS legislation

For more information, visit the website at http://www.premierfarnell.com