Premier Farnell shipping Two New PulsarPMOD Boards from ADI
Premier Farnell is now shipping the EVAL-ADT7420-PMDZ and the EVAL-ADXL355-PMDZ boards from ADI.
The Pmod (Peripheral Module) interface is an open standard specification used with FPGAs and microcontrollers. When prototyping, these boards are used in conjunction with the ADICUP360 (an Arduino form factor compatible ARM Cortex-M3 development platform) or the ADICUP3029 (an Arduino based wireless development platform for IoT applications based on an ultra-low power ARM Cortex-M3 processor). SPI and I2C PMOD peripheral connectors can also be found on many 3rd party MCU or FPGA development boards, where the PulsarPMOD board range can be connected directly into those systems, allowing you to develop your own code using ADI reference code found online.
The EVAL-ADT7420-PMDZ is a temperature measurement PMOD board accurate to 0.25 degrees Celsius. It has an I2C connector and is connectable to FPGA and MCU platforms.
The EVAL-ADXL355-PMDZ is a low noise, low drift 3-axis accelerometer PMOD board with 20-bit acceleration resolution and is also connectable to FPGA and MCU platforms.
Direct electrical and physical connections enable you to get started quickly with hardware and software, to help develop your solution.
These two PMOD compatible boards are now available from Farnell element14 in Europe, Newark element14 in North America and element14 in APAC. Visit the element14 Community for more information on the EVAL-ADT7420-PMDZ and the EVAL-ADXL355-PMDZ.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/