Leeds,
17
December
2019
|
00:45
Europe/Amsterdam

Renesas Electronics’ RA Family of 32-bit Arm Cortex-M based MCUs now available from Farnell

Renesas Advanced Family provides a high level of security, wide range of connectivity, low power consumption and scalability

FAR482_inline

Farnell, the Development Distributor, announces the availability of the RA Family of 32-bit Arm® Cortex®-M based MCUs from Renesas Electronics Corporation. This major product introduction will offer design engineers the flexibility to leverage Renesas’ ready to use partner solutions and Arm ecosystem whilst developing their own hardware and software solutions.

The RA MCUs include the advanced high-quality feature set that customers have come to expect from Renesas, with a special focus on security, connectivity and low power. They enable customers to deliver advanced solutions for a wide range of Internet of Things (IoT) applications, including industrial automation, cloud computing and IoT, building automation, smart environment, energy and metering, and home appliances.

All RA MCUs have been designed with a common DNA, making them feature-, software- and pin-compatible for easy scalability and code reuse from one device to another. It is now easy to develop IoT edge and endpoint devices, using the new Flexible Software Package (FSP), fast-start software for security and connectivity, and development tools from Renesas and the Arm partner ecosystem.

The RA MCUs deliver key advantages for design engineers such as market-leading embedded security, superior CoreMark® performance, and ultra-low power operation. Arm PSA security certification provides customers with the confidence and assurance to quickly deploy secure IoT endpoint and edge devices, and smart factory equipment for Industry 4.0.

Products now available from Farnell include:

  • The RA2 Series: This is the RA Family’s entry-level 32-bit MCU, offering excellent cost performance and ultra-low power consumption whilst delivering up to 48MHz of CPU performance. With cutting-edge peripherals such as capacitive touch, the RA2 is ideal for system control or user interface applications including healthcare devices, home appliances, office equipment and measuring equipment.
  • The RA4 Series: Satisfying the need for reasonable low power and the demand for connectivity and performance, this series offers a wide set of peripherals, including USB, CAN, ADC, capacitive touch, a segment LCD controller, and additional security IP integration. Suitable for a broad range of applications including industrial equipment, home appliances, office equipment, healthcare products and meters.
  • The RA6 Series: Offering the widest integration of communication interfaces as well as the best performance level - delivering up to 120MHz of CPU performance using an Arm Cortex-M4 core and a memory range from 512KB to 2MB Flash. This Series offers Ethernet, USB Full Speed and USB High Speed, QSPI, CAN, and TFT display driver integration. Its embedded Secure Crypto Engine is full of features that can be leveraged in higher-level solutions.

Lee Turner, Global Head of Semiconductors and SBC for Farnell says, “This is a significant new launch from Renesas, which provides our customers with greater options in the development of their IoT hardware and software, without compromising on key features such as security. This addition to our range means that customers can access our widest range of embedded solutions, whilst continuing to rely on Farnell for the latest in-stock products, alongside fast shipping and 24/5 technical support.”

The Renesas RA Family of 32-bit Arm® Cortex®-M based MCUs are in stock for same day dispatch from Farnell in EMEA, element14 in APAC, and Newark in North America.

Boilerplate

About us

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/