Skip navigation

Hussien Blog

10 posts
Introduction To Arduino Web Editor  In this simple video tutorial, it is explained to run it for the first time.   Hope this will be helpful for the newcomers.   ...
...
     In the market, there any many types of a potentiometer.  For a different application, we use different types of the potentiometer. Today we will look into the preset potentiometer with a knob. I like this the most because you don't need any tools to change the resistance. We make barely use our finger to change its value. Theoretically, the function of this potentiometer is the same as other potentiometers. The image below is the illustration of the potentiometer. ...
Arduino Tutorial #11:Simple Arduino Uno Shield For LCD Test                In this post, we shall see how can we can make a simple Arduino Uno shield to test HD44780 LCD. This shield can be used to test LCD 16x2 and as well as 20x4.               The reason for me to develop this test jig is because as a hobbyist I always have an issue when it come ...
                                                                               In our product review today, ...
     In the market, there any many types of potentiometer.  For a different application, we use different types of the potentiometer. Today we will look into the preset potentiometer with a knob. I like this the most because you don't need any tools to change the resistance. We make barely use our finger to change its value. Theoretically, the function of this potentiometer is the same as other potentiometers. The image below is the illustration of the potentiometer. ...
Arduino Tutorial #6: Introduction To Arduino Using Matlab Simulink                   In this tutorial, I would like to introduce you to the Arduino using the Matlab Simulink. Previously we have seen how to program an Arduino using the IDE. The process is pretty much the same, but the methods are different. The first thing you need to to do is to install the Matlab. The installation process is strai ...
Arduino Tutorial #4: RGB LED                   In this tutorial, we will look into how to control the RGB LED. First, let us look at the theoretical of the RGB LED. But before that, I would like to demonstrate how it will look when you test the LED with Arduino. Basically, an RGB LED is no difference from the normal LED, except that it has an addition of two more pins. And obviously, the internal st ...
In this tutorial, we will look at the readily available simulator for Arduino. There are a lot of simulators available in the market. Some need to be purchased and some are freeware, which means you can use it for free. Today we will look at the ArduUnoSim, which is a free simulator for Arduino. This software can be downloaded from the link below: Click Here For The Software Below is the screenshot of the ArduUnoSim This software is designed based on the Arduino Uno ( as the nam ...
Desoldering Pump   Last week I bought a desoldering pump from element14. The shipping took less than one week to arrive and it cost around RM 32.00. The manufacturer of this product is Duratool. This is the first time I am buying a product of this kind. Previously I used to use a pump and a soldering iron to desolder a component. By using this method it will take a while to get the job done. Sometimes it can get messy when you want to desolder an array of a pin from the printed circuit boar ...