Skip navigation
The Spot base platform features stereo cameras for obstacle avoidance, has a runtime of 90-minutes, and comes with customizable options. (Image credit: Boston Dynamics via YouTube)   Boston Dynamics has recently announced they are selling their popular Spot 4-legged robot, which has been in development for years. Annual videos released during that time have highlighted the robots seemingly unnatural capabilities, such as the infamous ‘kicking’ video released back in 2015. The c ...
Jeff Bezos and his plans to combat climate change Amazon CEO Jeff Bazos speaks at a press conference to unveil the companies plans to fight climate change. (Image Credit: AP Photo/Pablo Martinez Monsivais) On September 19th, Amazon CEO Jeff Bezos unveiled a new plan to help fight climate change called The Climate Pledge. The goal is to cut down on carbon emissions, becoming carbon-neutral by 2040, which is 10 years earlier than Paris’ goals. They are also aiming to have 80 percent of ...
University of Illinois (UI) researchers have developed minuscule soft robot machines, dubbed “the swimmer,” that are made of artificial and biological components that swim around when exposed to light.  It’s a promising development as it brings researchers in mechanical engineering one step closer to creating autonomous biobots. Their study has been published in the Proceedings in the National Academy of Sciences.   An artist’s rendering of the minuscule 1mm ...
The new plastic is 14 times stronger and eight times lighter than steel. This lightweight material was inspired by the mother of pearl. (Photo from University of Buffalo)   A return to indestructible plastic phones and devices? Yes, please.   Next to diamond, pearls are some of the most sought after jewels. They can represent anything from love to wealth, but a group of scientists is using the gems in a way that may change military armor. Researchers at the University at Buffalo, wit ...
Motoyasu Tanaka and his University of Electrocommunications research team based in Tokyo, Japan have developed a snake-like articulated robot that can move through narrow spaces and climb obstacles for search and rescue missions on disaster sites. This was difficult to achieve at first due to the amount of actuators in the system, but with the addition of three-dimensional steering, researchers are able to navigate the T2 Snake-3 a bit more precisely and easily than before.   The snake r ...
Japan’s unpiloted supply ship, HTV-8 (known as Kounotori8) was supposed to launch to the International Space Station on September 10th, but it was postponed due to a fire on the launch platform of the mission’s rocket. A new launch date has yet to be announced, and it won’t be expected until inspections and repair work is complete.   The H-2B rocket, built by the Mitsubishi Heavy Industries will be carrying the HTV-8 spacecraft to the International Space Station someti ...
Sam Battle, a London-based musician, programmer and owner of Look Mum No Computer YouTube channel, where he showcases various complex electronic instruments, like the organ made of 44 Furby toys, dedicated a large sum of his time building an entire ensemble out of musical instruments and LEGO Star Wars droids just by using BOOST 57253 Droid Commander.   The Star Wars droid orchestra consists of 42 musical instruments and 95 LEGO droids, all of which play at a certain time, composing John ...
Is this the future of extracting hydrogen? (mage credit: Getty Images)   A new discovery from a team of scientists may change the way we think about hydrogen. A group of Canadian engineers claims they have developed a way to extract hydrogen from oil without releasing greenhouse gases. The team says the technology has the potential to supply Canada’s entire electricity requirement for the next 220 years. Their research was presented at the Goldschmidt Geochemistry Conference in Barce ...
Russia’s Skybot F-380 is expected to perform a series of tasks under the control of cosmonaut Alexander Skvortsov. (Image credit: Roscosmos via Facebook)   Russia’s humanoid sometimes gunslinger robot Skybot F-380 has finally reached the ISS after the Soyuz capsule carrying it had difficulty docking with the ISS. The spacecraft aborted the docking procedure, which was scheduled for August 24th, when one of the components of the automatic docking port malfunctioned, which has sin ...
You wouldn’t normally expect to see a robot controlling a marionette in today’s technological world, especially because there’s little to no demand for these robots, and it would be very complex to develop such a system. However, that didn’t prevent ETH Zurich engineers from building a robot puppeteer that can be useful in warehouses or stores. Their results can be found in their technical paper.   While the puppet is moving in real life, the robot simulates the ...
Google’s subsidiary YouTube took down numerous videos of robot battles, like BattleBots, citing the content was in violation of the site’s terms of services, stating the videos showed acts of animal cruelty.   One of the videos that got removed features a battle between Speed Wedge and Ubersaw at the MassDestruction event. (Image Credit: Jamison Go, YouTube) The issue surfaced when Jamison Go, a competitor on the latest BattleBots season (team SawBlaze), was notified by Yo ...