shocking walls.jpg

A team from Hasso-Plattner-Institut create a new wearable using muscle stimulants to create walls in VR. The muscle stimulants simulate the fulling of resistance in objects. (Photo via Hasso-Plattner-Institut)

 

With VR technology integrated into full body suits, robotic hands, gloves, and exoskeletons, it’s becoming easier to mimic physical sensations. Even gaming sets like the HTC Vice does a good job at making you feel like you’re actually in the game you’re playing. But one thing VR hasn’t exactly nailed is creating impressions of realistic space. A team of researcher’s from Hasso-Plattner-Institut in Potsdam are looking to bring this experience to VR with their latest haptic system.

 

The team, led by Pedro Lopes, created a wearable setup made out of medical grade eight channel muscle simulators (EMS) installed in a backpack. The setup is controlled by a VR system that works with Samsung GearVR via USB. It also uses hand mount trackers and a motion capture system to track your movements. The electrodes are strapped on to your forearm, bicep, tricep, and shoulder on each arm. When you touch or lift a virtual object, a mild electric shock will automatically fire off giving you the feeling of weight and resistance of an object.

 

It took several tries for researchers to come up with a realistic simulation. After much trial and error, they eventually developed two different simulators. For the first one, they keep the EMS intensity at a certain limit. This let users interact with simulated objects by about 10 cm, which is ideal for soft things. For the second, a short EMS pulse was used and sent the user’s hand backward, preventing them from pushing through walls or other objects. And though the idea of using electric shocks for VR sounds scary, they aren’t strong enough to hurt you.

 

While using muscle stimulants for the VR experience is new, the technology itself isn’t. EMS is an essential part of physical therapy and training. Other companies are even finding ways of incorporating the technology for entertainment purposes, like Teslasuit. This is a full body suit for haptics in VR that relies on EMS. Lopes himself has even used the system for other projects, like feeling physical impacts in VR and an art project that forces users to keep cranking a machine lever due to EMS electrodes. He even tried to create barriers in VR three years ago, but wasn’t satisfied with the results.

 

Though the new system achieved favorable results, there’s still work to be done before it’s ready for the commercial market. For one, the team wants to streamline the design. Right now, the system is easy to wear, isn’t very big, and portable, but it’s not all that nice to look at. When the system finally is ready, it will bring us a step closer to a fully immersive VR experience. Imagine playing games and actually feeling the weight of objects or the sensation of brushing up against a wall. Is it necessary? Not really, but it may serve for a better VR experience. For now, you’ll have to rely on your imagination until the system is ready.

 

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell