25 SecondsThe first full working time-lapse shooting created with TIltPan Arduino Shield In the following video you see an example of time-lapse video with some scene movement created with the first prototype of the TiltPan Arduino Shield. There are three main scenes: curve diagonal movement from the bottom-left side to the upper-right, then the camera moves to the left pointing to reach the middle of the rotation horizontal plane. The last is a fixed scene pointing the sky. The entire sequence ...
Posted by
mcb1
Apr 3, 2015
Lights, Holiday and Electronics Earlier in the year Christian and element14 sent me the kit for the IoT Xmas Lights. http://www.element14.com/community/roadTests/1377 I was unable to enter in the challenge due to other commitments, so when I was offered the kit I promised to add something later. Lights I have an idea for the lights, and require to source some High Power LED's which the Infineon Shield can drive. Most of the existing strings are already voltage controlled ...