Skip navigation
In this Blog Download the Arduino software and power up the Uno and Due. Look at debug, does it exist from the Arduino GUI? See previous Blog… http://www.element14.com/community/groups/arduino/blog/2015/11/23/1-aardenergy-kick-off--a-new-project IDE Download IDE Down load from Uno board page, version 1.6.6 (I had already installed 1.6.5, so an upgrade). 1.6.5 uninstalled first, 1.6.6 now in place. However, under Tools>Board…Due is not listed. Get Started with Uno Use the ID ...
1. AardEnergy.   A Simple Plan Measure current and voltage on single phase electrical supplies Calculate electrical parameters like RMS, Real Power, Apparent Power, Power Factor, Frequency, THD, kWhr Use Arduino Uno with an electrical metering chip for parameters Use Arduino Due using software calculation of parameters Kick Off I’m new to Arduino but have used microcontrollers like PSoC4 and ARM Cortex-M3. Although my career has been more about hardware design I have written softwa ...
What is ? From a server to a SBC (Single Board Computer) or the board of your last robotic project it is not rare nor strange the need to keep the system and the container box under control avoiding excessive shocking vibrations, too much heating, adding a reliable digital power on/off system or reset automatically the entire device under certain conditions, as well as the availability of constantly updated parameters like the internal device temperature, the buttons pressed by the user (or stat ...
A new Arduino Gameboy called Arduboy. Nostalgia is fun, and nostalgic games are even more fun. Arduboy is a new and cheap ‘gameboy’ that allows you to play games old-school. (via Arduboy) I can't believe I missed out on this cute little gameboy-ish system powered by Arduino, with a heaping dose of nostalgia along with it. The creator, Kevin Bates, is calling it an Arduboy and he quit his full time job over a year ago to develop this creation. He even moved to China to get the pro ...

Filter Blog

By date: By tag: