Skip navigation
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   LoRa MER This is the landing page for my entry in the Build A Smarter World challenge featuring a prototype for a remote controlled vessel (LoRa Marine Environmental Ranger, or LoRa MER) that gathers environmental data and relays it to a shore based station using Arduino MKR WAN 1300 LoRa boards.  Approximately weekly ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I was lucky enough to get a MKR WiFi 1010  to add to my Robot ARM project I am modifying for the Arduino MKR Giveaway contest and the first thing I wanted to do was to get it connected to the local network. With the MKR1000 I have been using, I have used WiFi101 from the Arduino IDE for WiFi network examples.  Howev ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   This project is an entry in the Build a Smarter World MKR Fest. The challenge is to build a practical and useful system based on an arduino  MKR 1300. My plan is to build the MKR 1300 into a platform with a set of useful interfaces that allow it to be adapted to many applications. The core interfaces will be: a LoRa ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   Work in progress, semi daily blog, will post something more detailed later.   Entry 1 Using the CANReceiver sketch that comes with the CAN library. Started off with the CAN shield fitted, power from USB, no other CAN devices fitted. As it is, appears to be no signs on life in my serial terminal program, I'm using Handi ...

Filter Blog

By date: By tag: