Skip navigation
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   Introduction  Back in October (2018) I put forward an idea for making access to communal spaces smarter as my entry to the Arduino “MAKE A SMARTER WORLD COMPETITION”.   This blog documents my progress so far, of designing a smarter Access Control system based on two Arduino MKR WAN 1300 boards and a MKR ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I am building a prototype for a remote controlled vessel, the LoRa Marine Environmental Ranger (LoRa MER) that gathers environmental data and relays it to a shore based station using Arduino MKR WAN 1300 LoRa boards.  This post is the sixth in a series, and describes the boat afloat (but no power) and a DIY dipole antenn ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I am building a prototype for a remote controlled vessel, the LoRa Marine Environmental Ranger (LoRa MER) that gathers environmental data and relays it to a shore based station using Arduino MKR WAN 1300 LoRa boards.  This post is the fifth in a series, and describes the turbidity sensor and how the shore based station w ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I am building a prototype for a remote controlled vessel (LoRa Marine Environmental Reconnaissance, or LoRa MER) that gathers environmental data and relays it to a shore based station using Arduino MKR WAN 1300 LoRa boards.  This post is the fourth in a series, and describes the boat that will be used and a shore station ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I am prototyping an intelligent buoy (that evolved into a boat) that uses LoRa to communicate with a base station using the Arduino MKR WAN 1300 as part of the Build A Smarter World promotion by element14 and Arduino.  This post is the third in a series, and an extension of last week where the project began the movement ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   My idea was to give the LoRa capability to my old project The SolarBot (Simple Solar BOT  ----Finale ) and read the sensor data via LoRa. Another option can also be to control the SolarBot via LoRa Connectivity and I want to check out if this works without a lag in real-time. Then one can control the SolarBot remotely vi ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   Introduction   Today i will present the first steps of my project named "Detecting forestry fire focus, using Lora protocol".  The main objective of this project is create a tool for help firemen and foresters detect and contain fires, before they spread over the forest. In Brazil, this type of event occur practicall ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   I am prototyping a an Intelligent Buoy (that evolved into a boat) that uses LoRa to communicate with a base station using the Arduino MKR WAN 1300.  This post covers making a more robust prototype board for field testing and the issues encountered. Daughter Board All work up until now has been on breadboards and it i ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   The Project   CONECPT/iDEA: Fires in Industries have the most devastating effects. Just due to a flammable gas and a spark, a fire can occur causing a huge damage. Also now its necessary to monitor the status of the industry from anywhere. Be it home, for fire or police department or anywhere. I have an idea and tha ...

Filter Blog

By date: By tag: