Skip navigation

Arduino Projects

5 Posts authored by: BigG
NanoRama Enter Your Project for a chance to win a Nano Grand Prize bundle for the most innovative use of Arduino plus a $400 shopping cart! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   Introduction  Ireland, like much of the EU, is in lockdown and I now find myself locked out from using my Windows-10 laptop, which I need to use to complete my AVNET Guardian-100 MT3620 roadtest review. Yep, the wife and kids have commandeere ...
1.0    Introduction 2.0    Hardware The 1k NTAG Memory Map from I2C perspective 3.0    Firmware Decoding Text Messages Decoding URI Messages Decoding "Smart Poster" Messages Decoding MIME RTD Vcards Decoding MIME RTD Verb (application/vnd) Bluetooth details Decoding MIME RTD Verb (application/vnd) WiFi details 4.0    Demos     1.0    Introduction  This project st ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects     Introduction  This is the follow up to my previous blog "Smarter Access Control using Arduino MKR WAN 1300 boards" which forms part of my entry to the Arduino “MAKE A SMARTER WORLD COMPETITION”.   Let me start by saying that my overall objective for this project is to showcase the breadth of the ...
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects   Introduction  Back in October (2018) I put forward an idea for making access to communal spaces smarter as my entry to the Arduino “MAKE A SMARTER WORLD COMPETITION”.   This blog documents my progress so far, of designing a smarter Access Control system based on two Arduino MKR WAN 1300 boards and a MKR ...
Introduction  This is my idea to develop a smart device, using the Arduino MKR WAN 1300 Board, which will help make access to communal spaces smarter. The reason for this blog was to put forward a proposal for the "Build a Smarter World" contest.     Problem to be addressed  There has always been a dilemma on how to manage public amenities effectively. One the one hand, if amenities have open access and are not monitored then anti-social problems tend to arise. While on t ...

Filter Blog

By date: By tag: