Skip navigation
As part of a project to build a digital rotary table I've been experimenting with double height characters.   The Circuit The circuit for this is an I2C LCD display wired to the standard I2C pins on the Arduino and a linear 10K potentiometer with the wiper connected to the analogue input 0 on the Aruduino. In the code   The setup function creates a few blocky custom characters. An array stores the defintions of the numbers 0-9 with regards to which of those custom characters ne ...
The new Arduino integration for Atmel Studio takes under 10 minutes to install and provides a fully compatible Arduino programming tool.   Atmel Studio is a free version of Microsoft Visual Studio. The Arduino plugin is also free, although an optional Arduino usb debugger license can currently be purchased for $15 (rrp $49)   All versions of Arduino are supported, although Arduino 1.5 is currently beta. The single installer also suppports visual studio pro 2008, 2010, 2012 and atmel ...
Learn with Arno Shield... A where to begin complete learning platform (via Olympia Circuits)   As many people already know, the Arduino is a versatile platform. It is a great place to start when learning about embedded electronics, or a great stepping-stone to learning about electronics in general. However, some people still struggle to begin with the Arduino and may have difficulties building and connecting circuits for the first time. Peter Gould and Kevin Warner recognized this when the ...

Filter Blog

By date: By tag: