Skip navigation
Can anybody tell me how to configure an SD card, wifi-shield, and the serial monitor to all work simultaneously??? I'm trying to capture an image using motion detection and, afterwards, save the array of 100 images to the SD card.  Afterwards, I hope to use the wifi-shield to push a notification to an app from OpenCV code. Is this possible? ...
Everything that happens on a micro-controller has to be known. This includes dealing with memory. Many people (myself included) have developed a wonderful set of code that can dynamically use and free memory through the standard malloc and free functions. Only later do we discover that our available memory is getting reduced as time goes by -- followed by undetermined and random failures.   This is because no microcontroller (the Arduino included) has the ability to garbage collect.   ...
User interfaces can take up a lot of memory. That is why, while developing the Arduino User Interface I focused on developing a way to store things in Program Memory instead. It turns out that storing -- and then using -- program memory objects can be slightly confusing. So I thought I would write a quick post about it.   Most people are familiar with the simple use of program memory for strings. Instead of writing   Serial.println("This is taking up a lot of mem"); &# ...
One of my first big micro-controller projects was called the Neonatal Closed Loop Oxygen System. When babies are born prematurely, they have to be fed very specific amounts of oxygen. Too little oxygen and they suffocate, too much oxygen and they can die from oxygen toxicity. Current methods are not advanced, essentially involving a nurse adjusting the oxygen levels manually. The goal of the project was to develop an automatic system.   We had to prevent this little guy from getting oxygen ...
     For many years Morse code was a large part of the mandatory licensing examination in both Canada and the US. In order to get a basic license to transmit on amateur bands, a prospective amateur would have to commit him or herself to learning Morse code. This was likely a large reason why many interested in amateur radio failed to ever complete or even take their exam.              In late 2006, the Federal Communic ...

Filter Blog

By date: By tag: