Skip navigation
Madhu here for the weekly post..   I wanted to try out something cool and inexpensive. So I bought this Buzzer online. To make this work I hooked it up to the Arduino PWM signal pins, which runs at around 500 Hz (would be ideal to produce audible tone). I love creating electrical circuits using Fritzing and created this to show the circuit that I used. For the Simulink part - Once I found out that Arduino has functions tone and noTone, I set up a S-function builder block in Simulink th ...
Anuja Apte

"Make" this Halloween

Posted by Anuja Apte Oct 24, 2014
Hey! It's Madhu Govindarajan here - For this week’s blog post, I will share some ideas for makers who want to get creative with their Halloween celebrations. The few things that pop-up to mind when thinking about Halloween – Trick or treat, carving pumpkins and haunted house attractions. A custom Speech to Text converting script can be implemented with ease on Raspberry pi. This can be used to identify someone saying “Trick or treat” which can control an automatic Ca ...
LCD Interfaced with Arduino and Controlled by MATLAB   ...
I would like to introduce you to Madhu Govindarajan from MathWorks who will be writing interesting blog posts for next several weeks. Thanks Madhu! Hi everyone! Madhu here - I thought for today’s post I will share the answer to a frequently asked question during the recent Autonomous Fighting Robots Challenge (AFRC). Flexibility to build and expand existing solutions is one of key aspects fueling the Maker movement. I want to share how Simulink in essence supports the same thought proce ...
A fun new project for you Arduino enthusiasts!       The code, a block diagram and a photo are posted below. enjoy!   SUMMARY This demo is a wireless display that can be updated remotely using a web browser on your phone, tablet or PC connected tohttp://goHACK.me   HARDWARE Wi-Fi AMW004-E03 Mackerel board from ACKme Networks Display 1.2" 8x8 Matrix LED from Adafruit Arduino: Mega2560 (other Arduinos ok too, but must be 3.3V) DESCRIPTION After the Mackerel boa ...
Proteus + Arduino + Serial Controlled DC Motor (A Prototype for Robot)     Real Hardware and Software Combination.  Robot Which is controlled by Android/ Smart Phone over Bluetooth.   Major Hardware: 1. Arduino Borad Atmega328 2. Bluetooth Module (HC-05) 3. Motor Driver L293D and Two Geared DC Motors.   ...
After the success of GestureR, Grabo Team is going to present our next Kickstarter project – BLEasy. BLEasy is a Revolutionary, Easy-to-use and One-to-many BLE (Bluetooth Low Energy) bridge for your Arduino System.     The launch day for BLEasy would be on 3rd Oct 2014. For the details, you may click on the following link for a preview: https://www.kickstarter.com/projects/grabo/930856984?token=f710ece1   If you are interested in BLEasy, please don’t hesitate to sup ...

Filter Blog

By date: By tag: