Skip navigation
  The ESP8266 is a low-cost Wi-Fi chip with full TCP/IP stack and microcontroller capability produced by Shanghai-based Chinese manufacturer, Espressif Systems.The chip first came to the attention of western makers in August 2014 with the ESP-01 module, made by a third-party manufacturer, AI-Thinker. This small module allows microcontrollers to connect to a Wi-Fi network and make simple TCP/IP connections using Hayes-style commands. However, at the time there was almost no English-language ...
This blog documents some belated progress on my Star Trek themed Pi IoT design challenge entry. It is being put in the arduino area since that is where it is most useful. I wanted to make the subsystems useful and built well enough to work reliably in their target environment, so this sensor array is built using a custom PCB. The PCB did not arrive until well after the challenge was over, but it worked perfectly with no errors when I assembled it. The card features an arduino pro micro which ...
I've been looking into designing my own Arduino programming and development board after seeing Ben Heck's episode. Apologies if this is in the wrong area.   So I made a quick Schematic in Eagle using the arduino schematic from the website, I've included support for the ATTiny85. I know this isn't the first time someone has done something like this, or with home pcb manufacture, just wanted to share some of the problems I've had with this design.   So here is the final result, I don't ...

Ublox Neo-6m from E-Bay

Posted by ajens23 Nov 9, 2016
Ublox Neo-6M  from E-bay Hi All,   (First time trying this so please forgive if it's in the wrong place/format/whatever)   Just received a couple of Ublox Neo-6M GPS boards from E-bay and thought I would try a quick review for anyone interested. Board: GY-GPS6MV2 with Ublox Neo-6M Seller: Worldchips Shipping: included Price: 17USD(+/-) Apparently this board contains a voltage regulator (5 pin chip to left of RX/TX pins) and can be powered off of a 5V supply. I am usin ...

Filter Blog

By date: By tag: