Skip navigation
This is my first use of transistors in a project. I need to control a SainSmart 16-Channel Relay Module using an Arduino 101(3v3 GPIOs). This Relay Module uses 5 vdc through Opto couplers to power the relays. The input pins on the relay board are at 4.4 vdc and need to be brought to GND to switch on. When I connected the Arduino 101(3v3 GPIOs) directly to the relay module some of the relays would stay on while others would be controlled by the Arduino. It all worked fine when I tried an Arduino ...
This video is all about interfacing BMP180 module with Arduino. BMP180 will help us to measure environmental temperature  and pressure and by using that we can calculate the altitude which can be used in various applications like weather monitoring, navigation etc. The BMP180 sensor module comes with I2C interface and with a default address 0x77 which is not configurable limiting stacking of multiple modules to that same I2C bus. In this tutorial we will interface the module with Arduino by ...
What do you thing about this project? Have you some interesting ideas for expansion?   ...

Filter Blog

By date: By tag: