Skip navigation
The proposal will reclassify internet service as information service, rendering the Title II regulations obsolete. The faces of its demise. (Image credit FCC)   The FCC has released its final draft on the net neutrality issue under the title “Restoring Internet Freedom,” with the proposal expected to pass during the Open Meeting December 14 vote. The draft essentially reverses/repeals the net neutrality protections implemented during the Obama administration back in 2015 by doi ...
Digital currency is on the fast track to phase out physical money, which poses several problems that will be costly in the long run. (Image credit Flickr)   One word comes to mind when thinking about digital currency ─ convenience. It’s easy to carry, doesn’t wear out and is accepted nearly everywhere. According to a 2015 report from the Federal Reserve, only 32% of consumers in the US used cash for their purchases in 2015, an 8% decrease from 2012 and the numbers continue to d ...
Shutter Controller for Testing Control Prototype Assembly Software Design Commands The MotorControl Class The Arduino Sketch Previous article Next article   According to the PONF Project design, the digital camera back will use a digital shutter controlled independently by an Infineon microcontroller - at the date, our ideas are focused on the XMC1100 IC - hosting an Infineon TLE94112LE DC motor controller. These two components and the shutter itself ...
Programming Application Notes Software Sources Videocore IV Data Acquisition How the Camera Sensor Works 24Mp Image Sensor Approach References and Available Documentation Changes and Upgrades Software Driver Sensor Control Software Previous article Next article Programming Application Notes These notes define a scenario illustrating the application strategy we will follow to enable the Compute Module 3 to interface the 24Mp Sony sensor of the PONF came ...
The $900 bundle includes the Rift, a pair of Touch controllers, three sensors and three facial interfaces. (Image credit Oculus)   Oculus announced earlier this month that the VR company was releasing a bundle package aimed at businesses in an effort to help companies build their own VR experiences for clients and customers. The Facebook-owned platform envisions businesses using the Rift for a variety of applications, including collaboration and training in several different industries. &ld ...

Filter Blog

By date: By tag: