Skip navigation
When the Raspberry Pi was introduced in the classroom as a viable desktop replacement, many were skeptical to the processing power and software ecosystem that came with the single board computer. Then came the Pitop and things have never been the same. Enter Computex 2019 on 26th May in Taipei, where the future of technology is showcased and one of the unexpected demos was Qualcomm Snapdragon 8cx and it's partnership with Lenovo. Codenamed Project Limitless, a 2-in-1 laptop was on display that i ...
I find stories like these inspirational. They are poised for a big success. Even older companies can make a splash like a startup.   A two decade-year old software developer company called Panic has unveiled a new handheld video game system known as Playdate. It comes bundled with a hand crank that can be used as an option to play video games. Playdate is only available in yellow, is small enough to fit in your pocket, has a black and white screen and can play a variety of games. The handh ...
The Long Term Stock Exchange was recently approved by the SEC and could change how tech startups go public. The LTSE could bring big chances to the stock market. (Stock Photo)   Every year we hear about the latest promising tech startup. By the end of the year, we hear of another one shutting down. If only these companies had enough time to develop their products, without worrying about profit growth. They may get that chance.   U.S. regulators recently approved a new stock exchange ...
The high end designer showed of their “Canvas of the Future” during their Cruise 2020 runway show. These may be innovative, but they’re not very pretty. (Image credit: Louis Vuitton)   High-end fashion designers are always looking for the next cutting edge trend, especially when it comes to technology. Louis Vuitton recently hopped on board with their latest bag that features built-in flexible displays. Dubbed the “Canvas Bag of the Future,” the handbags were ...
Google has leased with Hudson Pacific Properties to convert Los Angeles’ Westside Pavilion mall into an office campus, which will also generate foot traffic and revenue for any remaining stores. (Image credit: Hudson Pacific Properties)   Shopping malls in America have been shuttering their doors for years since online retail stores have become more popular with consumers. Business Insider predicts that 75,000 stores will close across North America by 2024, and that’s on top of ...
Not only is self-assembly bot manufacturing inexpensive, they’re faster to build and easy to transport. The MIT team used a five-legged robot to test the new technique. (Photo from MIT)   Robots have a multitude of uses that can help with various applications, but they’re not necessarily easy to make on a mass scale. It’s a time-consuming task that requires the proper steps to ensure their mechanical parts, electronics, and sensors are installed properly. To help address ...
With the promise of new 5G technology on the horizon, there is no doubt that electronics companies are faced with new challenges to meet the demands of the higher performance technology, and it’s a race too. These challenges are being faced by test and measurement companies, integrated circuit design companies, as well as PCB and interconnect companies. The trouble stems from the high frequencies 5G needs to operate at, to provide the speed and low latency it has promised.   The fre ...

Filter Blog

By date: By tag: