Project InformationProject Description: https://green-scientist.com/projects/1-meter-of-pi-2pi-microgravity-garden/ 1 Meter of Pi Project Blog: 1 Meter of Pi Github repo: https://github.com/kurama007/1MeterOfPi IntroductionIt is already No 9 blog post and time goes by very quickly. It is almost the end of the year 2020. Hope everyone is safe and healthy. As this 1 meter of pi project is near the end, I would like to make this project useful for other people. Our customers can be ast ...
A very short update: there are more and more sprouts, however they are growing slower than I expected and there are a lot of sprouts on the wrong side of the vase. Need more light? YES, the problem was definitely that the amount of light provided by LED strips (mounted on the edges of the Gr0G cube) and by the high efficiency grow LEDs (mounted on a standpoint in the middle of the cube) is not enough So the only quick-and-dirty solution I can apply right now is to provide more current ...
CONSTRUCTING THE BOT Robo Arm: The above picture shows the unassembled parts of the robo arm with 4 DOF. And the arm looks like this after the build or assembly. Base of the Bot: The above picture shows the unassembled parts of the Base with 2 DOF. And the base chasis looks like this after the build or assembly. I'm just using two wheels, for simple operation. Now, It's time to connect the robo arm and the base. And after connecting the things, the bot will look like t ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Enclosure Prototype I found a 0.5m3 cardboard shipping box in the garage and repurposed it into my enclosure prototype. While the enclosure can certainly accommodate 32 pot systems, I chose to prototype with only 8 so I could focus on quality experimentation over quantity. More on the ...
As we all know, lighting is important. It's crucial to plant development- Ok I'm going to skip that boring intro since we all know plants need water yada yada yada. I mean, I could talk about photocells and phosphorus and photosynthesis and whatever else is involved, and that would waste 30 minutes of your time. To prevent boredom, let's jump straight into today's progress. Here, let's get a visual aid first! Well I did complain abou ...
BLOG# 10 -Edible Algae System - (Growing Spirulina in space) Application Implementation and Tests This is my 10th blog post in a series of blog post for the Design Challenge 1 Meter of Pi version 1.1 ,<<< PREVIOUS BLOG NEX BLOG >> Blog# 9 Developmental Unit Testing Blog# 11 EAS - Conclusions and Enhancements for Future Systems INTRODUCTION In this blog I will attempt to Code and test the Workflows described in Blog#7 First, I will show some pictures of the growin ...
We've already taken a look into the contents of the challenger kit. Now lets get started with the components of the kit. Getting Started with Raspberry Pi 4: Before getting started we need some hardware and software components, they are: Hardware: Raspberry Pi 4 Micro SD card ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
The whole Mushrooms' Paradise blog
Power supply
Raspberry PI
Enviro HAT
Humidifier components.
Fan components.
LED strips.
Power supply The power supply is an ATX PSU with 24-pin cable. The power connector pinout Detailed description can be found here: ATX Power Supply Pinout and Connectors. Basically all back wires are Ground, yellow - 12V, Orange - 3.3V, Red - 5V. Note: green wire - PS_ON needs to be connected to the Ground for the p ...
The whole blog
The Wiring Pi package
GPIO Utility
Allow connection to PI desktop GUI without monitor
The Wiring Pi package The Wiring PI package contains the GPIO utility which I can use from the Terminal to debug wiring issues. The Wiring Pi package was not installed with my PI by default, so I needed to install it manually. Instructions to do so can be found here: wiringPi updated to 2.52 for the Raspberry Pi 4B. Basically the commands to be run from T ...
Almost done with assembly! Here: Front view, powered off. Power structure: There are two 110V AC plugs required. One is a cable extender to power pi and arduino, and one for the pump. I figured it might be a good idea for manual power cut to the pump. As you can see on one of the later images, the Pi is booted with the python script running. Here's how you can set it up, to run the script upon boot. We'll using somethin ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
In the last Blogs, I have already mentioned somewhat details of what I am going to do for this 1m3Pi Challange, I loved working on the MQTT protocol. There are two BME280 sensors that are sending data with ESPs. For the debugging purpose, I wanted to have all the sensors data on the LCD screen, which also looks nicer if I would make it somewhat fancier. Nevertheless, I also tried to start both LCDs together but the LCD on the Enviro Hat isn't starting. The problem could be in ...
Previous Blog Project R.A.G. - Blog #5 - Sensor & Light Module Blog #6 - Mechanical Build P1 - Robot On Rails
1. Introduction
2. Idea
3. Plan
4. Design
Wheel assembly
Wheel
Adapter
Wheel body
Finished Wheel
Wheel Mount 1
Wheel Mount 2
Finished wheel assembly
Belt & motor assembly
Motor Mount
Flat surface mount
20x20 extrusion mount
Belt Tensioner
Bushing
Gear holder
Flat surface mount
20x20 extrusion mount ...
The whole blog I will have roughly half of the components controlled by the RPI and half by the ESP32. RPI components are controlling mushrooms part of the farm, ESP32 - vegetable part. This entry is about the components controlled by the Raspberry PI. This is the set before being assembled. It contains: 1 Raspberry PI 4 heat sinks for RPI 1 Enviro HAT 3 computer fans 3 LED strips 1 Humidifier 1 IOT Relay for humidifier 2 5V relays for LEDs and for fans 1 ATX PSU (power supply un ...
WELL It worked! Here's some video demos. This is the one with the full op. version, infinitely on: (I originally did CDN but ralph said that was a download and since I accidentally clicked image which had 10mb limit, I thought it was not possible) Here's the one with a 6 hour delay Oh gosh what a short blog Hey does anyone want to chat about random stuff? Uhh... to fill up this blog? Hmm... I'm goi ...
Welllll Relays are very interesting. I'm setting up one right now, with an arduino uno. I've set the setting for 1 second of high-stream water dispense, per every 6 hours. Here's the code. int RelayPin = 12;
void setup() {
// Set RelayPin as an output pin
pinMode(RelayPin, OUTPUT);
}
void loop() {
// Let's turn on the relay...
digitalWrite(RelayPin, LOW);
delay(21600000);
// Let's turn off the relay... ...
Design Features: This is a modular and scalable design. More water tanks can be added at any time and a single or more water tank can be removed easily from the system for harvesting the required amount of algae at a time. Valves at the end of each water tank for the maintenance and scalability of the system Each water container is to be half-filled with water and half with used capsules of air. As the algae grow and photosynthesis occurs, it will replenish the oxygen level in the air. ...
BLOG# 9 -Edible Algae System - (Growing Spirulina in space) Developmental Unit Testing This is my 9th blog post in a series of blog post for the Design Challenge 1 Meter of Pi Updated version 1.2 ,<<< PREVIOUS BLOG NEX BLOG >> Blog# 8.2 (Part 2 of 2) EAS - DATA REPOSITORY MongoDB Blog# 10 Application Implementation and Tests INTRODUCTION This blog will describe the Unit Test done on each component of the system the test will be broken into 2 groups Electronic and Softwar ...
Previous Blog Project R.A.G. - Blog #4 - Quick Tool Change Mechanism For The Robot Arm Blog #5 - Sensor & Light Module
1. Introduction
2. Idea
Sensors
Lights
3. Plan
Sensors I'm planning on using
MQ135
DHT22
Phototransistor
LED strips
What kind of light do we need?
Control circuit
4. Design
Enclosure
MQ135 Mount
DTH22 Mount
7 Segment Display Mount
Connectors
Electronics
Schematic
Perfboard
5. Final Build ...
BLOG# 8.2 -Edible Algae System - (Growing Spirulina in space) System Build This is Part 2 of my 8th blog post in a series of blog post for the Design Challenge 1 Meter of Pi version 1.2 <<< PREVIOUS BLOG NEXT BLOG >>> Blog# 8.1 (Part 1 of 2) EAS - System Build Blog# 9 EAS - Electrical and Class Unit Testing INTRODUCTION In this blog, I will introduce you to the database that is used to persist the telemetry data generated by the EAS system MongoDB will be used ...
BLOG# 8.1 -Edible Algae System - (Growing Spirulina in space) System Build This is Part 1 of my 8th blog post in a series of blog post for the Design Challenge 1 Meter of Pi version 1.1 ,<<< PREVIOUS BLOG NEXT BLOG >>> Blog# 7 System Designs -- Software Design Blog# 8.2 (Part 2 of 2) EAS - DATA REPOSITORY MongoDB INTRODUCTION Ok, here we are on the 9th of December the year 2020. I'm on the home stretch. As of today, the Challenge Page Dates states, tha ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials How The Challenger Kit Will Be Used This is my first time using Raspberry Pi so it will be quite a challenge, but I'm excited to learn! Raspberry Pi 4 2GB The Raspberry Pi will execute automation code and store data. PIM487 (Automation HAT Mini) The Automation HAT will automate the irrigation system. PIM486 ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design The Project Plan: T-minus — 10 Weeks Now that I have a design, it's time to create my project plan, a roadmap for how my design will become a prototype! Research The problems addressed by the project will be researched The challenge kit of parts will be researched with respect to using them in the project System Design Plant pot design Chamber enclosure d ...
Merry Christmas all ! Hope everyone is safe and sound. Welcome to a new update on the Space Vegetables Project. Not much has changed from last time, but here's the latest updates. Nutrients Although the PPM has not changed much, I'm following the General Hydro (the Nutrients manufacturer) instructions. This is the 6th week, so, I'm changing proportions of the nutrients - as the plants grow, so they needs change - the need less of some nutrients and need more of oth ...
Procrastination is, indeed very useful. I'll just claim the past 20 days were spent on uhh.... growing plants... 5 blog posts in the next 10 days. Sounds... not too impossible. Oh, I also installed the enclosure, and, added the pi in and ran initial testing. Seems all good. Wait it's 6. *Elf14 can we *please* have a smol' extension* *puppy eyes* *puppy eyes intensifies* Wait in electronics we do cats *cute kitten e ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors The Space Salad System Concept: Three Delicious and Nutritious Meals a Day Having outlined how to grow plants in microgravity, I can now focus on what types of plants to grow as well as the spatial arrangement of the plants. The goal is to feed and nourish a rocketship crew so what came to my mind right away was salad! (Salad lettuce is a no-brainer because it is so easy and quick to grow!) I call my conc ...
My Background Hello! My name is Anthony Neil Tan and I am a UC Berkeley Bioengineering undergraduate. Last year, I competed in NASA's Growing Beyond Earth (GBE) maker contest with the goal of becoming a better engineer. 1 Meter of Pi is surprisingly similar to GBE, but this time around, 1 Meter of Pi is an individual challenge. I won't have engineering team members to fall back on, but instead I will have the opportunity to face challenges head-on and develop a newfound confidence in my enginee ...
Here is a list of previous posts Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 12 - Building the high-pressure system Gr0G - 14 - Piping Gr0G ...
We are already in the second half of the project and we want to see how we can help astronauts with this 1 meter of Pi project. So far, during this project, we realized that there are a couple of challenges in microgravity garden. Let's recap a couple of challenges that we want to solve with this project! 1. Non self-pollinating plants need pollination --> how to monitor them and help pollination mechanically, bugs, or wind 2. We want to avoid bugs in space --> Bug c ...
In this blog I will be setting up the Raspberry Pi. I got the Raspberry Pi 4 (2GB) when I got selected as a challenger. Then I bought the official raspberry pi type-C power supply and a 32GB micro SD card. I followed the following steps to setup the device: 1. Download the latest Raspbian OS image and the 'Raspberry Pi Imager'. 2. Flash the SD card with the Raspbian OS image. This created two partitions of the SD card. Boot files are written in the partition with name 'boot'. I did ...
Hi all ! Hope everyone is safe and sound. This little update is to share how I read the TDS value of the nutrients solution and make it available to the Space Vegetables Client. Hardware The sensor is from DF Robot . It measures the Total Dissolved Solids. It indicates how many milligrams of soluble solids are dissolved in one liter of water. EC and TDS EC stands for Electrical Conductivity and TDS stands for Total Dissolved Solids (already explained above). They both are widely ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! Ne ...
I have been doing some research to do the lighting of the plants effectively. They are called plant grow lights to name it. I came across many new terms and methods used to illuminate plants Indore or even in space. The plants grow with photons(light particles) being thrown on them at constant or varying intensity depending on their needs. Light intensity or how densely packed light is with Photons is measured with Mico-moles per meter square per seconds or PPFD(Photosynthetic Photon ...
I have developed the basic principles of motion and control for one of the most important aspects of my design proposals, the ‘GIZZMOTO’ special pump with a telescopic outlet/extension and a distribution head attachment. The purpose of the system is to give the options of supplying Air – at ambient or increased temperature – or Moisture, in the form of atomised droplets – again, at a pre-set temperature – to each of four levels, where growing containers ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
Previous Blog Project R.A.G. - Blog #3 - Lift Off Blog #4 - Quick Tool Change Mechanism For The Robot Arm
1. Introduction
2. Idea
3. Plan
4. Design
Off the shelf components
SG90 Servo
Screw 1
Screw 2
Spring
Custom made parts
Base
Motor Mount
Barrel
Pistons
Cap
Sleeve Template
Finished Assembly
5. Finished mechanism
6. Servo Tester
7. Testing
8. Further development
9. Fun news from the ISS
10. What's next? ...
Previous Blog Project R.A.G. - Blog #2 - Strapped In For Launch - Connectors Blog #3 - Lift Off
1. Introduction
2. What's in the Starter Kit?
Raspberry Pi 4 2GB
Pimoroni Automation Hat
Pimoroni Enviro Hat
Pimoroni PICO Hat Hacker
3. What am I gonna use from the Starter Kit?
4. Main unit and PDU idea
5. Fun news from the ISS
6. What's next?
7. Summary
1. Introduction Hi! This will be my third blog for the 1 Meter of Pi D ...
'As your rocket ship blasts into space, speeding to Mars, you have 1m3 of space to grow your food and nutrients for the journey. Resources are limited, and you need to make it work!' Well, nobody will ever wish this to happen with them. But in case if it ever happens with me during my 'Space Odyssey', where will I find the food? It is obvious that I will not find Dominos there in the space. So, what is the solution? It would be nearly impossible to find any place in the space where food ...
Hello ! Hope all are safe and sound. This is the last post about the software that drives the Space Vegetables Project - the client. More info on the design: Space Vegetables - #5 : System concept and design Space Vegetables - #6 : Software Design Space Vegetables - #10 | Software #0: Wiring and Python programs The Space Vegetables server post I'm going to split this post into 2 - this one is about the SpaceVetetablesClient.py and the other will talk about the TDS sen ...
The whole blog
Hardware
Steps for configuring PI
Steps for configuring ESP32
(Optional) Configuring VNC
HardwareMy Raspberry PI model is 4B with 4GB RAM My ESP32 model is NodeMCU-32S My laptop is Intel Core i5 and has Windows 10 Home OS. Maybe I will need to add something there in the future, but so far the configuration steps are below, with links to detailed instructions on each step. Steps for configuring PI Download Pi Imager fo ...
Welcome all to the latest update for Space Vegetables. Hope all are safe. This week I've changed some things around the greenhouse because the vegetables are growing well. I'm guessing by the time the Astronauts reach Mars, they'll be able to eat something ! The vegetables are growing beautifully. You can't smell through the Internet, but they smell wonderful. The tomatoes smell is my favorite. I'm now able to identify all the vegetables in the hydroponics ki ...
In my last blog, I explained the working of both the Hats connected with pi using the Pico Hat Hacker. There is only one BME temperature/Humidity sensor is connected with this kind of connection. My idea was to have more sensors at different places of the 1m3 space to monitor the environment effectively. In fact the research shows that the Plant growing chamber currently on IIS in space has more than 180 different types of sensors to monitor the environment effectively also with IR camera to h ...
Completing the last stages of scale-model construction to form a Power Module that sits at a foundations/ground level: The special pump/base/tank assembly is affixed in the centre of the bottom housing A-MVF-GIZZMOTO & BASE MTG.jpg An Air Compressor is positioned on one side and an Air Receiver on the opposite side. B-MVF POWER MODULE ISO VIEW 1.jpg C-MVF POWER MODULE ISO VIEW 2.jpg In this instance the piece of equipment has a 12-volts DC motor (*) An a ...
Here is a list of previous posts Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - 14 - Piping G ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
Previous Blog Posts ...Blog #1: 2Pi Microgravity Garden Blog 1 | Getting Started | element14 | 1 Meter of Pi Blog #2: 2Pi Microgravity Garden Blog 2 | Raspberry Pi s... | element14 | 1 Meter of Pi Blog #3: 2Pi Microgravity Garden Blog 3 | Hello World wi... | element14 | 1 Meter of Pi Blog #4: 2Pi Microgravity Garden Blog 4 | Software Envir... | element14 | 1 Meter of Pi Blog #5: 2Pi Microgravity Garden Blog 5 | Connect to Arduino and how plants get pollinated inside rocket without wind??? Blog ...
Hi all ! Hope everyone is well and safe. This is the update on the server side of Space Vegetables. More info on the design: Space Vegetables - #5 : System concept and design Space Vegetables - #6 : Software Design Space Vegetables - #10 | Software #0: Wiring and Python programs Hardware This is connected to a Raspberry PI 3B+ with the Automation HAT MINI from the KIT, that's connected to the water and air pump and the lights. Software The "serve ...
Since my last blog on Construction, I have been focusing on Item 4 on the list of Main Elements. Bringing to the fore the need to maintain good growing conditions, I have spent a huge amount of time working on an automated system – eventually to be controlled by a Raspberry Pi 4 and PIM 487/486/300 assembly - to provide controlled levels of moisture/water, humidity, and adjustable temperatures - and I think I have an answer: ‘GIZZMOTO’ a no-moving parts pump with a telescopic o ...
BLOG# 7 -Edible Algae System - (Growing Spirulina in space) System Designs -- Software Design This is my 7th blog post in a series of blog post for the Design Challenge 1 Meter of Pi version 1.2 ,<<< PREVIOUS BLOG NEX BLOG >> Blog# 6 EAS - System Designs -- Block diagram Blog# 8.1 (Part 1 of 2) EAS - System Build INTRODUCTION This blog will describe all the software and programming used in the system. The main focus will be to describe the OS, Database, Libraries, ...
Hello all ! Hope all be safe and sound. Welcome to the third update for the Space Vegetables Project. Plants The plants are growing well, although I'm sensing a pattern and don't know why - or at least, don't know if it's from it. The plants in the top layer are growing bigger than the ones on the bottom. The lights are the same and they are at the same distance from them (at least, apparently). They are the same quality - at least some, and they don't show the sam ...
Hi all ! Hope everyone is safe and sound ! This post is just to share the contraption I made to read the PH level of the water. Because the PH sensor cannot stay in water for long - like the TDS sensor - I've build a small contraption to read the PH level and display it in a TFT screen I had laying around. Here's the schematics of the build: The build is nothing fancy - a small wooden box with holes to the power button Code To be ab ...
Previous Blog Project R.A.G. - Blog #1 - Mission Briefing Blog #2 - Strapped In For Launch - Connectors
1. Introduction
For what do I need connectors?
Requirements List
Previous Work
2. Waterproof Connector
Idea
Design
3.5mm variant
Barrel jack variant (5.5/2.1mm)
Finished Connector
3.Magnetic Connector
Idea
Design
Finished Connector
4. Conclusion
5. Fun news from the ISS
6. What's next?
7. Summary
1. Introdu ...
The whole blog For vegetables part of the garden I chose lettuce and radishes, I explained the choice in Part #1 ( Mushrooms' Paradise #1 - Initial Plan | element14 | 1 Meter of Pi) of the blog. The vegetable part of the garden will be at the bottom of the enclosure, in planters. For Lettuce, after some research (for example, growing facts How to grow lettuce indoors? An easy step-by-step guide – Bulbo® and growing instructions Growing Lettuce Indoors Year-Round ...
1 Meter of Pi Blog Posts ...Blog #1: 2Pi Microgravity Garden Blog 1 | Getting Started | element14 | 1 Meter of PiBlog #2: 2Pi Microgravity Garden Blog 2 | Raspberry Pi s... | element14 | 1 Meter of Pi Blog #3: 2Pi Microgravity Garden Blog 3 | Hello World wi... | element14 | 1 Meter of Pi Blog #4: 2Pi Microgravity Garden Blog 4 | Software Envir... | element14 | 1 Meter of Pi Blog #5: 2Pi Microgravity Garden Blog 5 | Connect to Arduino and how plants get pollinated inside rocket without wind??? ...
The whole blog I plan to use Raspberry PI and ESP 32 as controlling devices - the brains of the project; Enviro for temperature and humidity sensors, humidifier, 4 soil moisture sensors for vegetables part of enclosure, 4 fans for ventilation, 4 water pumps for irrigation, several LED strips as growing light. RPI will control Enviro, fans and humidifier. ESP 32 will control the soil moisture sensors and pumps. ESP 32 will communicate with the PI using MQTT. Optionally (if I will be abl ...
Hello all. Hope everyone is ok and safe. In this series of posts I will describe how everything is wired, connected and talks with each other . The following image shows what each Raspberry PI controls and how everything is wired Relay 4 channels I had to use a relay because the Air Pump is 220v and the Automation Hat MINI cannot handle that much voltage. Although the lights are 12v, my first attempts to control the lights just using the outputs we ...
Unboxing: The kit arrived in a nice package. The package includes the following items: Raspberry Pi 4 B 2GB PIM486 ENVIRO Hat PIM487 Automation Hat Mini PIM300 PICO Hat Hacker
Inroduction In this blog post, I am going to walk you through the hardware I am going to use for the Pi-ski-farmer which includes - Raspberry Pi 4(2GB version) Pimorini Enviro Hat Pimorini Automation Hat Pimorini Hacker shield Husky Lens Raspberry Pi 4(2GB version) There are already countless sources of information on getting to know the Raspberry Pi 4 on the internet. However, for sake of completion, I will cover that here. The Raspberry Pi 4 is a single board computer for ho ...
The Wait is OVER!! The wait was long and the wait was hard. Day after day I used to see other challengers doing cool things with their kits while I used to haggle with Customs officials over the delivery details for my package. At one point I thought that I would not be able to take part in the challenge but then almost a month later I finally did receive the package and Oh boy!! It was one of the most wonderful packages I ever received from the community. The packaging was great as usual and ...
Here is a list of the posts in this challenge Gr0G - 01 - Introduction Gr0G - 02 - Why aeroponics? Gr0G - 03 - High-pressure system design Gr0G - 04 - Mechanical design Gr0G - 05 - Electrical design Gr0G - 06 - Building the box Gr0G - 07 - Playing with the Gertbot Gr0G - 08 - Installing LEDs Gr0G - 09 - The control board Gr0G - 10 - Software design Gr0G - 11 - Building the box (2) Gr0G - 12 - Building the high-pressure system Gr0G - 13 - Building the high-pressure system (2) Gr0G - ...
Ok! My procrastination has lead to me not doing anything. Well, I managed to get the Enviro hat to work. This blog will document my progress. Initially: I didn't have a HDMI monitor free, I had a Raspberry PI Foundation 7" touchscreen, but didn't really use it. I just used it to check the IP address and unplugged. This is using SSH. SSH by default is disabled on the Pi. You must go to pi configuration and set it to on, and then reboot. Here is how to conne ...