Hello all ! Hope everyone is felling well and safe. Although 1 meter of PI Design Challenge is officially over, I will keep posting until I have some vegetables out of it ! The plants are growing well, and the tomatoes are already touching the top of the greenhouse. I know I can trim them to keep them from growing taller. There's been a rough days for temperature in my city. Thermometers are hinting temperatures below 0ºc , but in the greenhouse the temper ...
In my previous blog, you all learnt this is a simple control system that uses water, ventilation and light to grow plants in modular cells, In this blog let's connect everything and run it. Here's the logo of the Agrocube Let's get started: Use a 12V power source preferably a 12V battery so that it won't have a problem with electricity issues in developing country like India/Africa. This 12V will be used power the pump and also for LED's if required. So here's the connection diagram: ...
I will use these last two blogs to only document the project I have done so far. Though I feel that there is still many things on which I could improve, add more components and code but I am happy with what I was able to do in this challenge. There are currently the following parts of the project. Raspberry Pi 4B Pimoroni Automation HaT Pimoroni Enviro HaT DPS310 Sensor ESP8266 + BME280 (MQTT Publishing) WemosD1R1 + BME280 (MQTT Publishing) Esp32 Pico V4 + RGB LED Strip (M ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Blog 5 - Enclosure Prototype + Light/Air/Temperature Blog 6 - Plant Pot System + Assembly Blog 7 - Enviro HAT Data Collection and Plotting Blog 8 - Automation HAT Irrigation System Blog 9 - Wearing Two HATs At Once Reflection This challenge sped by really fast! In this short amount of ...
Got my automation mini hat working now. Yay! excited to write this after a gap. Completely got delayed due to various circumstances, but I just don't want to give up. My plants didn't sprout properly due to 2 reasons one the seed I chose was spinach which is a spring crop unfortunately and took more time to come out due to cold winter here in Bengaluru. The second reason is the soil used was dense and might pressurise the seeds to stay in maybe ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
Previous Blog Project R.A.G. - Blog #10 - Mechanical Build P3 (Final) The Robot Assisted Garden Project
1. Introduction
2. Software
I2C Communication
Master
Slave
GUI
Finished code
Raspberry code
SL Module code
WR Module code
3. Final Tests
Controlling the lights through the GUI
Controlling the robot over the GUI
Controlling the pump over the GUI
4. Through the blogs
Blog #1 --- Mission Briefing
Blog #2 --- Strapped In For Launch - ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Blog 5 - Enclosure Prototype + Light/Air/Temperature Blog 6 - Plant Pot System + Assembly Blog 7 - Enviro HAT Data Collection and Plotting Blog 8 - Automation HAT Irrigation System Wearing Two HATs At Once This time I decided to have a playful pun as the blog title, as it aptly descri ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Blog 5 - Enclosure Prototype + Light/Air/Temperature Blog 6 - Plant Pot System + Assembly Blog 7 - Enviro HAT Data Collection and Plotting Automation HAT Setup The Automation HAT is an attachment that perfectly snaps onto the Pi pins. It is outfitted with inputs and outputs that allow ...
The system makes use of the already available hardware in the challenger kit, with some additional items. Let me list out all the items necessary. Raspberry Pi 4 MAX30102 sensor Pimoroni PIM487 Automation HAT PIM486 Enviro HAT PICO HAT Hacker PCB Insulated Copper wires for Anode and cathode linkage to the power supply Hot glue cylindrical pipe - a small piece Wire mesh Rubber tube O2 suction mask Buzzer RGB LED Power Bank DC power supply The blood oxygen leve ...
Approaches: Oxygen generator for a whole area (currently limited due to resource constraints) Portable oxygen generator for an individual (this project focuses on this) For approach 1, good quality atmospheric oxygen PPM sensors are costly and are out of our financial budget. One such module is AST SRZ-CA24-4 from OxyCheq. For our demonstration, we use approach 2 where we use a MAX30102 Pulse Oximeter & Heart Rate Monitor sensor from Maxim Integrated. C ...
Aim: This project aims to tackle an emergency event of oxygen deficiency. In confined and restricted spaces, be it even a safe bunker/shelter during a global disaster, a workspace, or a rocket ship speeding to space and beyond, humans if present, will be needed to sustain the amount of oxygen for a prolonged period of time, within their body as well as the surrounding space. If personnel more than the allowed number are present in a confined space, oxygen can easily run out within that ...
In the last blog as I have mentioned, I got the box ready, now it is time for assembling the parts. In the next two blogs, I will explain the full project in detail with the code. I assembled the LED lights on the top. Set the color of the lights to purple. Then it was time to put the RPI into the field. Here, I am using a power bank to power up the Pi. I am also placing the ESP's connected with BME280 sensors on the both of the sidewalls of the 1m3 of space. Here, in the thir ...
Hi all ! Hope everyone is well and fine. It has been a challenging couple of months . Thinking of the project, assembling the greenhouse, putting everything together, testing and production - it has been a wonderful ride. Always had a special interest in hydroponics and this project was the perfect excuse to try it. I know it's not scientifically accurate - but NASA has spent millions to be able to grow radish in the International Space Station - and I don't have that kind of b ...
The autonomous pest management will take care of the elimination of flora and fauna pests in limited or confined cultivation. The system consists of a Rpi 4 which acts as the brain. A Rpi cam connected to the Rpi4 will detect the presence of any pests via OpenCV and machine learning models. The PIM486 Enviro HAT will additionally detect any change in the ambient temperature, humidity, pressure, etc which can lead to plant decay. The PIM487 Automation HAT will control a set of servo mo ...
Introduction and motivation This project introduces a novel concept of pest management in closed spaces such as space farming. Be it a bunker or space vehicle with very limited space to spare, plant cultivation would be a major task, if the people inside the bunker/space vehicle are to survive for an extended amount of time. This also includes enclosed or partly enclosed structures on farms such as silos, vats, tanks, pits, etc. But, with closed space cultivation has its adv ...
Project InformationProject Description: https://green-scientist.com/projects/1-meter-of-pi-2pi-microgravity-garden/ 1 Meter of Pi Project Blog: 1 Meter of Pi Github repo: https://github.com/kurama007/1MeterOfPi Objective of This 1 meter of Pi ProjectJust as a reminder, the objective of this project is to demonstrate a working prototype to grow vegetables to feed astronauts inside 1 cubic meter. The challenges that we faced in this environment are 1. Constantly provide water 2. Non- ...
Below is the random writings throughout the project and well.......I decided this is a portion of the project book I created that has all my sketches and information in it. For fun here it is more ramblings...... Entry #1 Sept 2nd. The first thing I wanted to do in this design challenge was to get my thoughts in order. To start planning the adventure, to document as much as I could. As I wo ...
It's been a long journey and I have plans for more to come when it comes to my build so the fun doesn't stop here. I noticed when rendering my video a bunch of my video decided it would mess up so I have a few smaller shorter videos and information coming in regards to the project. I will say I was looking for a fun project for the winter months. This certainly fit the bill on that one. I didn't realized how fun it was going to be, I have learned a lot about pushing the limits ...
Like any project there is always alternatives that can be done. I had thought a lot about this project prior to starting. I was certainly trying to find out a way to make this project the most cost efficient and easy to build so basically anyone anywhere could reproduce it and be able to add on to it without any issues. With most of our projects I am sure I am not the only one that is guilty of this and that is over thinking everything. When I started I had tons of ideas and th ...
Previous Blog Project R.A.G. - Blog #9 - Water & Rail Module Blog #10 - Mechanical Build P3 (Final)
1. Introduction
2. Previously done
Blog #6 --- Mechanical Build P1
Blog #8 --- Mechanical Build P2
3. Plan for this blog
4. Design
Materials
Light mount structure
3D printed mounts
Mount 1
Mount 2
Mount 3
Mounting the electronics
Pipe mount
Module mount
5. Assembly
6. Finished Build
7. What's next?
8. Fun news from the I ...
The estimated setup is as follows: * Rpi will be stacked with Rpi cam, PICO HAT Hacker PCB, PIM486 Enviro HAT, and PIM487 Automation HAT. * It will contribute to roughly L * W * H as 86 * 57 * (25 + 17 + 9) = 86 * 57 * 51 (mm) ...
* As the theme of this design challenge goes, this project focuses on the sustainability of mankind in case of a global disaster or that of an interplanetary voyage. * The project is developed to have an autonomous self-contained system for plant cultivation so that the least human intervention is required for maintenance. * It is not only small in terms if footprint size, but it will be so small that multiple of these can be developed with ease and be put in various congested spaces within th ...
The whole Mushrooms' Paradise blog
Components
ESP32
DIY Irrigation kit
Soil moisture sensors.
Water pumps
3.3v Relays
And the problem
This post is about the vegetable part of the farm. This part doesn’t use anything from Element14 kit, but I thought it could be a nice add-on to mushrooms farm. Components ESP32 Vegetable part of the farm will be controlled by ESP32. I chose ESP32 because I will need analog pins for ...
INSTALLATION OF LIGHTS Before moving on to the final stages – Schematic Design of the Complete System and Schematic Design of Controls – I installed LED lighting and configured the Operational Controls, with an additional indication feature: MVF LIGHTS OFF, jpg MVF LIGHTS ON .jpg I have made a small video clip that also makes the lighting more apparent, with the addition of a flashing warning light, signalling the telescopic drive is in operation. MVF LIGHTS ON .mov Next, the ...
The whole blog
Introduction
Step 1. Rehydrating the mushroom cakes
Step 2. Preparation of Vermiculite and Perlite
Step 3. Putting mushrooms on the trays
Introduction To grow mushrooms I used the “PF Tek” method. Full description on how to do it can be found here: Start To Finish “PF Tek” For Growing Mushrooms At Home (Part 1) Start To Finish "PF Tek" For Growing Mushrooms At Home (Part 2) I already did the initial part of it ...
Addendum A to Blog/Post Nine: I previously wrote: “Note: In the original proposal I had included a Solar Panel (or a series of panels) to be sited at the very top of the Construction to provide additional back-up power.” ADDS: As the application is indoors, today’s technology would not be practical. However, tomorrow’s technology could change that perspective: There are at least two areas of research from which practical experiments are pointing the way to ...
I was working on making a Box for putting the sensors and Pi as well as lights which have a relatively nice encloser. I went to one of the friends who could make such a box of a Wood I don't know how good I was in building the box and also in the main part which was the automation of lights for 1m3 of Pi, but let's have a look at some of the photos. I am also going to add the Peltier cooling system for the 1m3 of Pi Space. For that I bought TEC1-12706 module. Norma ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Blog 5 - Enclosure Prototype + Light/Air/Temperature Blog 6 - Plant Pot System + Assembly Raspberry Pi Setup Here's a great video by Crosstalk Solutions that shows how to set up the Raspberry Pi. Watch from start up to 21:20 for Pi configuration and SSH setup. Download SSH client PuTT ...
This is the last blog required, as well as the last one documenting major changes.. This blog includes my final thoughts, and potential future direction. Let's first jump into what I did in the past few days. I've made the system's pump system with a small container that stores water. It looks large at 16.9OZ (it's totally not a Pepsi bottle! Totally not!) but it is rather small considering the strength of the pump. Here's the video demonstration of the pump blasting out ...
Previous Blog Project R.A.G. - Blog #8 - Mechanical Build P2 - Robot On Rails Blog #9 - Water & Rail Module
1. Introduction
2. Idea & Plan
3. Design
Electronics
Relay circuit
Circuit
Test
3 pin HC-SR04
Circuit
Code
Test
Motor driver circuit
Multiplexer circuit
Circuit
CD4051BE
Test circuit
Test
Full schematic
Soldering the perfboard
Enclosure
4 pin 3D printed connector
4. Software
5. Testing the mod ...
The whole blog For the enclosure I used an old non-working fridge. Mushrooms and vegetables will grow inside the fridge, electronics are located just next to it. The reason for electronics to be outside is I need RPI to be able to connect to WiFi and it will be not possible from inside of metal fridge. The access side of the enclosure is covered with plastic film, to make humidification more efficient. Here are the dimensions. Fridge seems to be pretty big, so I thought it ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
The whole Mushrooms' Paradise blog
3v Relays
IoT Relay
Other
The final result
Demo run
Data visualization by ThingSpeak
Components (continued from Mushrooms' Paradise #9. PI components review in detail. Part 1 ) 3v RelaysThere were not a lot of 3v relays options. I got mine here and they don’t have any specifications listed. But it looks like they need less than 16mA, otherwise they will not work. IoT RelayIt is used to run a humidifie ...
So I decided I would add to the front panel it worked pretty good it's all sealed up on the inside and I just used some green tape to seal the front doors up. So we should be good and sealed up now. I will however shortly here have to get some more air circulation going on in the unit but that shouldn't take too long. Yup it's most certainly time to cut that glow down a bit. Yup that should do the trick. I will be adding another panel to the side there and also get the ot ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
So now I have my watering system all setup its time to get to the planting so where do we begin. I decided to use peat pucks for planting the seed as given anywhere nutrients and everything can be added to a system after the fact but getting the seeds started in a environment they are most likely to succeed was the thing I wanted to attend to first. Mind you I wanted to be able to have the soil go to the top of my containers so I could have even holes on to when the plastic was over ...
When it comes to working the bugs out there is many things to think of first we have hardware related bugs things that won't work and then software issues where things wont work with what we have installed for hardware. This can sometimes be challenging when using something like software that has been created by someone else where one could make a more simple setup work just as efficient but we have to consider time and resources and what is needed to be done to complete and get things goi ...
When it came to the software I was really wanting to try out some software I had seen which if I could do it over I would have done something differently but due to time and so much going on it wasn't in the books. I had to make something work even tho it was a bit of a pain. So I decided to use TerrariumPi currently it is only able to be run headless on the raspberry pi 4. You can check out TerrariumPi over on GitHub here: https://github.com/theyosh/TerrariumPI ...
When I started with the electronics I scoured around my workshop to pull all the parts out of bins to see what I go, low and behold I had some items. But not sure how or if they will work I decided to go ahead with the project of getting the electronics together. I ordered some cheap parts as well and off to the races I went frantically trying to get things together. Finding out things didn't work and purchased items were not labelled correctly on the listings causing som ...
The whole Mushrooms' Paradise blog
The whole Python code
Code explanations
Imported Libraries and classes
Classes
Common properties for all the classes
Common methods for all the classes
Code for lights
Code for fan
Code for Humidifier
Initialization of ThingSpeak data
Main loop
Error handling code
This project has 3 types of components: mushrooms specific, vegetables specific and common. Mushrooms specific components are ...
BLOG# 11 - Edible Algae System - (Growing Spirulina in space) Conclusions and Enhancements for future systems This is my FINAL blog post in a series of blog post for the Design Challenge 1 Meter of Pi version 1.1 ,<<< PREVIOUS BLOG Blog# 10 System Application Tests INTRODUCTION This is my last blog for the Design Challenge "1 Meter of PI". It was an interesting journey for me. I gained a tremendous amount of knowledge about the Raspberry PI softeware development platform ...
Posted by
dules Jan 2, 2021
Unfortunate turn of events I was planning a build sprint from Christmas to the end of the contest on my off days for holidays. Did a lot of research, planned everything and gathered all the required materials (covid-19 definitely made that difficult). But unfortunately my region (Croatia - Sisak/Petrinja) got hit with few strong earthquakes, the biggest one being 6.4 Richter. My family is ok, and luckily my house was built strong and 20km away from the epicenter so we didn't hav ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
Hi everyone ! Hope you all had a great Christmas and a Happy New Year. Another weekly update, but with a bit more this week. We all know that the project timeline is ending, but I'm going to keep posting here until the first vegetables are harvested from the project. I will not end it on January 5th. Fruiting We have bean pods starting to grow ! The lettuce and other vegetables are also growing well. Code I'm still having some "ghosts" t ...
latepost 1meterofpi Hello everyone, I had received hardware a bit late due to customs issue and delivery delays due to covid-19. This is a late post, everything recorded below is actually been tested and implemented during the first week of November but could not post the blog due to various reasons. I have received the following hardware: 1. Raspberry pi 2GB 2. Pimoroni Enviro 486 kit 3. Automation HAT mini And I bought the following hardware 1. Wate ...
As I am going to use RGB LED strips to provide proper lights to my plants, I have started to do experiments with the strips I have. The LED strip is 2m long with 60Leds/m. Each LED consumes approx ~60 mAmps. This means the entire strip would need approximately 7.2 Amps. The Led strip needs a standard 5V supply. So the adapter like the one in the below picture should work to supply the required Watts to the strip. Now, the RGB Led's have +(plus) and -(minus) as well as DIN pin to sen ...
Previous Blog Posts Blog 1 - Challenge Overview + Plant Growth Factors Blog 2 - Plant Growth Chamber Design Blog 3 - The Project Plan + Prototype Materials Blog 4 - Automation Using The Challenger Kit Blog 5 - Enclosure Prototype + Light/Air/Temperature In this blog, I'll describe my plant pot system and explain how it satisfies the relevant plant growth factors. I'll also demonstrate how my plant pot system innovates upon existing methods. Plant Pot System According to the ...
Previous blogs Description #1 - Introduction, the plan and materials preparation In this blog post we describe the project's main concept and some initial high-level design of it. #2 - Materials and casing assembly Our journey with selecting proper materials, cutting and assembling the drawer and its casing! #3 - Modelling, cutting, planting! The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables! #4 - Plan ...
Previous Blog Project R.A.G. - Blog #7 - The Mainframe - P1 Blog #8 - Mechanical Build P2 - Robot On Rails
1. Introduction
2. Plan for this blog
3. Rail system
Problems from last time
Setting the Vref
Protecting the driver
New mount for the motor
Testing the rail system
4. Robot surgery
5. Testing the motion system
6. What's next?
7. Fun news from the ISS
8. Summary
1. Introduction Hi! This will be my eighth blog for t ...
Previous Blog Project R.A.G. - Blog #6 - Mechanical Build P1 - Robot On Rails Blog #7 - The Mainframe - P1
1. Introduction
2. Idea
3. Plan
4. Design
Enclosure
Power In Panel
Bottom Panel
Side Panel
Enviro Hat Mount
Electronics
12V/5V switcher
Relay circuit
Schottky circuit
Soldering the perfboard
Testing with Arduino
Testing with the Raspberry
I2C breakout
Common ground breakout
5. Assembly
12V PSU
Main box
Panel ...