Skip navigation
The whole Mushrooms' Paradise blog   So I think it will be the last post for this blog. After software and hardware modifications the mushroom farm started to produce healthy mushrooms!   Just a couple of interesting notes: Mushroom cakes do not fruit all at once as I expected. Some mushrooms pop up, I will pick them up and in several days more mushrooms pop up, even without the rehydration of the cakes. I read that if mycelium is disturbed on the cake, for example scraped with a for ...
The whole Mushrooms' Paradise blog   Here is a short update on the mushrooms' farm.   Unfortunately, the first batch of mushrooms died. I think my EnviroHAT was a bit defective and was showing humidity much higher than it really was. My code used to check humidity and turn humidifier only if it is lower than needed. So I assume it was getting wrong readings and didn't run humidifier often enough. Some mushrooms' cakes from the first batch did sprout but then all of them dried out. ...
feiticeir0

Space Vegetables - #27

Posted by feiticeir0 Mar 16, 2021
  Hi all ! Hope everyone is well.   Here's another update on the project. I'm going to keep doing these because the project is still ongoing until I get to eat something grown there !   Greenhouse Because the weather is improving each day (still, a bit of rain is expected) and getting warmer, I've moved the project from my garage to my terrace. No more lightning, but no more automation and no more time lapses. The water pump is now on a timer - 30 minutes every 1h:30m . Now, ...
  Hello all.   Hope everyone is safe and sound.   Here's another update from the Space Vegetables project.   Vegetables are growing well, especially the salads. Any day now and I'm able to harvest some to try. Tomatoes and Bell peppers are still small... I'm hopping the sunny and warm days will improve and give a boost to their growth . Probably by the end of March will move the kit to outside and spare the electricity bill on the LEDs.   I'm worrying that the botto ...