The autonomous pest management will take care of the elimination of flora and fauna pests in limited or confined cultivation. The system consists of a Rpi 4 which acts as the brain. A Rpi cam connected to the Rpi4 will detect the presence of any pests via OpenCV and machine learning models. The PIM486 Enviro HAT will additionally detect any change in the ambient temperature, humidity, pressure, etc which can lead to plant decay. The PIM487 Automation HAT will control a set of servo mo ...
Introduction and motivation This project introduces a novel concept of pest management in closed spaces such as space farming. Be it a bunker or space vehicle with very limited space to spare, plant cultivation would be a major task, if the people inside the bunker/space vehicle are to survive for an extended amount of time. This also includes enclosed or partly enclosed structures on farms such as silos, vats, tanks, pits, etc. But, with closed space cultivation has its adv ...