Design Features: This is a modular and scalable design. More water tanks can be added at any time and a single or more water tank can be removed easily from the system for harvesting the required amount of algae at a time. Valves at the end of each water tank for the maintenance and scalability of the system Each water container is to be half-filled with water and half with used capsules of air. As the algae grow and photosynthesis occurs, it will replenish the oxygen level in the air. ...
After a terrific series of events at Space, we are all geared up to do more research here to learn about the lifeform that we are going to grow. Earlier, in 1. SPACE CRASHHH... and need to grow food to survive! Whhat??, we had fully convinced ourselves that we'd harvest Spirulina, so today's research matter would mostly include what kind of environmental conditions are a must for us to maintain healthy growth of these algae systems. This research is essential to designing a ...
As much as we hope this happens to none...but we gotta be prepared. Crisis doesn't come telling. This is about preparing for the odds that we wish never occur.. such as the ongoing pandemic, falling short of eatables in space, run out of food in a water expedition. These aren't easy situations at any level but we're exactly going to try to solve such a situation..by Tech! So the present situation is... I, along with my crew of 5 other people had flown using our spaceship to clos ...