Skip navigation
Here are my previous posts for the BBB Radio Challenge:   Beaglebone Black Internet Radio Challenge - onebeartoe - Unboxing and Project Goals http://www.element14.com/community/roadTestReviews/1695 Beaglebone Black Internet Radio Challenge - onebeartoe - Installing FM Support     This project was really fun to work on.  I hadn't used a BeagleBone Black before, and wish I could have used more if it GPIO features.  I did have experience writing Java code for Raspberry ...
So as I mentioned, I was planning to make two projects. As the first one took a long time, I just had a couple of days to finish this one and publish it. Unfortunately, it didn't work due to couple of reasons: Initial plan was to write some sort of wrapper to rtl_adsb and display an offline map as popular dump1090 uses Google Maps API and needs Internet connection. I was running out of time so decided to use dump1090 instead. So map displaying needs a WiFi connection. Small screen meant that I ...
The playback interface was missing in my previous version of the BBBRadio. So I added it using wxMediaCtrl.   Below is the updated screen for main GUI of BBBRadio.   Click on WavPlayer to open the interface to the media control.     The media control interface consists of simple elements such as Open File - for opening the file Filename TextBox - for displaying the filename Delete - for deleting the file displayed on the Filename textbox Play - play selected file ...