Welcome to another installment in the Design Challenge Weekly Summary series here at Element14! It’s week Five of the IoT On Wheels Challenge, and things are getting off to a great start. Before we jump into the challenge, you should take a moment and read my intro post that will fill you in on the full details of the challenge as well as the challengers who are competing to win some amazing prizes. Additionally, there will be a listing at the bottom of this post with links to my previous coverage of this challenge.

 

 

IoT On Wheels Design Challenge

 

 

About The Challenge

 

 

Featured as the third design challenge of 2017, the IoT On Wheels Design Challenge opened for project idea submissions in June of 2017, which was met with many submissions from community members. As I mentioned earlier, the challenge is based around the NUCLEO-L476RG development boardNUCLEO-L476RG development board which is built on the STM32L4STM32L4 Arm Cortex M4 line of processors. Challengers have ten weeks to develop their project, and share their progress in a series of weekly update post. By posting a minimum of ten update post, challengers become eligible to win several awesome prizes, and the chance to become one of our prestigious design challenge winners.

 

 

Entering the challenge is not limited to just the ten chosen community members though,  anyone can join the Challenge as a non-sponsored Challenger. Here's how: Simply get the low-cost NUCLEO-L476RGNUCLEO-L476RG and integrate it into your project, as well as post 10 blogs about your design journey in the IoT on Wheels space (tagging your blogs 'IoT on Wheels'). All Challengers must build their projects in accordance with the Challenge's terms and conditions and all projects must include the  NUCLEO-L476RGNUCLEO-L476RG

 

 

The Official Kit, and The Prizes

 

 

On September 4th, 2017 Element14 announced which 10 community members were picked to participate in this challenge, and those 10 challengers received a kit of sponsored components to use in their design which was sponsored by STMicroelectronics. Each kit contains the following items:

 

 

To learn more about each of these components or to purchase them to use in your own project, visit the official kit announcement at the links above.

 

Each challenger is competing to win one of three prize packs that feature prizes ranging from a Segway Mini Pro, to an Oculus Rift VR headset, Bicycle GPS system, GoPro Hero 5, and even a radio controlled hobby truck. Other prizes include tools from Duratool, a bench power supply, and even a high end pair of headphones. All challengers who complete ten blog post and finish their project will also receive a prize pack including a tool kit from Duratool, a heat gun, and digital multi-meter. These prizes are open to all who enter the challenge, despite not being an official challenger, with the requirements being the same: Use a STMicro NUCLEO-L47RG and post ten blog post by the challenge’s deadline on November 13th.

 

 

The Past Week In Review

 

Over the past 7 days, October 8 - October 14, we have had a total of nine updates posted across seven projects. Before we get to my highlights for this week, let's take a look at which projects were updated this week!

 

 

 

This Week’s Top Updates

 

 

Project: Smart Drive - Exploring MEMS board X-NUCLEO-IKS01A2 with Unicleo-GUI - Blog #3

 

 

This week was full of great blog post, and the one that really stood out for me was the third update to project Smart Drive. In this post, Sergei Vlasov (vlasov01) walked us through the methods he used to begin logging data such as fall detection, environmental metrics and more using the X-NUCLEO-IKS01A2X-NUCLEO-IKS01A2 expansion board. The X-CUBE-MEMS1 software package was used for standalone data logging as it includes a fall detection library negating the need to write something custom. This update is full of useful information, and I would highly suggest checking it out at the link above.

 

 

Project: Smart Bike, Smart Rider - NexTion Enhanced Heven SbSr

 

 

In its second update, project Smart Bike , Smart Rider saw a fairly interesting display added into its hardware list. The Nextion display is designed to make GUI design easier for those who wish to add a display to their embedded project. Until this project, I had not heard of these displays, but from what I can tell, they are actually pretty useful for projects where a small touch-screen display is needed. The display’s real advantage comes into play with the Nextion Editor, a drag and drop GUI builder, that is capable of creating some pretty robust layouts. Learn more about this display, and how Gurinder Singh (gsgill112)is using it in his project at the link above.

 

 

Project: Fatigue Alert System (Blog #3)

 

 

Our final highlight this week comes from project Fatigue Alert System by Dale Winhold (dwinhold). In the project’s third update Dale clued us onto some issues he was having with the Nucleo-64 boardNucleo-64 board. He’s having issues with his computer recognizing the board when plugged in, and is hoping some community members can lend some troubleshooting advice. He also showcased his plan to use capacitive sensing to determine if the driver of the vehicle’s hands are touching the steering wheel, and sounding an alert if the system detects that the driver's hands have left the steering wheel.  If you think you can be of assistance in troubleshooting the issues Dale has been experiencing, head over to the link above and drop him a comment.

 

 

That is going to wrap up things for this week, tune in next week for another Design Challenge Summary. If you would like to learn more about this challenge, and to see what progress has already been made, head over to the its official challenge page, and as always, remember to hack the world and make awesome!

Weekly Summaries About This Challenge

  1. Design Challenge Weekly Summary: Intro to the IoT On Wheels ChallengeDesign Challenge Weekly Summary: Intro to the IoT On Wheels Challenge
  2. Design Challenge Weekly Summary: September 6 - September 16, 2017
  3. Design Challenge Weekly Summary: September 17 - September 23, 2017
  4. Design Challenge Weekly Summary: September 24 - September 30, 2017
  5. Design Challenge Weekly Summary: October 1 - October 7, 2017
  6. Design Challenge Weekly Summary: October 8 - October 14, 2017
  7. Design Challenge Weekly Summary: October 15 - October 21, 2017
  8. Design Challenge Weekly Summary: October 22 - October 28, 2017
  9. Design Challenge Weekly Summary: November 5 - November 11, 2017
  10. Design Challenge Weekly Summary: November 12 - November 18, 2017 Final Week
  11. IoT On Wheels Design Challenge Summary