Agriculture is one of the noble profession by which one can feed themselves and also produce enough to feed others. At the end of the day it boils down to the food, in order to live we need food and we cannot eat money! It's very dangerous to see that trend that is been affecting the farmlands which are being converted into urban ecosystems and Special Economic Zones or SEZ. Which are one of the main reasons for the increase in commodity prices and global warming. Even ...
Problem : Ubiquitous smartphone access has empowered almost every individual with access to information and services that make our lives not only make daily life easy But almost enables us to do and perform at much higher levels. However, The switch to touch screen as the primary means of input for phones has created a barrier for a large community of visually impaired users from using a smartphone to its full potential. The Touch-Tying accessibility function on android phones usin ...