Previous Blog:  Design for a Cause - The Ultimate Smart Trike Design Blog 1 of 4

 

BILL OF MATERIALS (FOR THIS PART OF THE BUILD)

In this episode, we convert the mechanical aspects of the trike to electric.  We are not tackling the "Smart" electronics at this stage.  We first need to understand the challenges ahead once we test ride it still dumb and dangerous.

 

The motor controller and throttle weren't worth a build as they are very inexpensive to purchase.  Since our build spanned multiple disciplines, not everything we needed was on Newark, so I included the raw specs with this BOM:

 

650W, 36V, 450RPM Output Geared Motor

34 Tooth Sprocket

#40 Chain

15mm bore freewheel

36V Thumb Throttle and Motor Controller

(3)18Ah Batteries Product LinkProduct Link

Molex  36663-000136663-0001 Product LinkProduct Link

Molex 36664-0001 Product LinkProduct Link

Molex  50-84-102050-84-1020 Product LinkProduct Link

Molex  50-84-202050-84-2020 Product LinkProduct Link

(2) Inline Fuse Holders

(2) 25 A Fuses

3" x 3/16" Carbon Steal plate

1/4"x 20 Grade 8 bolting

Dual Piston Brake caliper and hydraulic actuator (as found on ATVs)

Zip ties

 

 

MOUNTING THE MOTOR

After assessing the Trike and mocking up its rear carriage in Autodesk Fusion 360, we elected to mount the motor to a 3/16" plate that was then bolted to the top bracing of the carriage.  It allowed for a direct shot for the new chain after cutting the trike basket.  It also would allow for installing the batteries low to keep the center of gravity of the trike low.

 

Smart Trike Concept Motor Installation

 

We found there was not enough clearance to install the new sprocket.  So, we elected to eliminate the original band brake at that center location and install a disk brake at the drive wheel.  We plan to make this actuate from the MKR1000 versus by cable.

 

We wired the 3 batteries in series to create a 36V power source.

TEST DRIVE

It assembled nicely and Connor took the motorized for a test drive in its l dumb and dangerous state.

 

The test drive identified the following hazards:

  • You could easily run over your legs with the back wheels if you accidently hit the throttle when stopped with your feet down.
  • In a panic, its hard not to remember to take your thumb off the throttle while braking.
  • The original brakes do not stop the trike quickly enough.
  • The trike has to take wide turns.  Tight turns that you would do on a bike will actually cause it to go up on one wheel in the back.  This is not a problem for the paved rail trails we ride, but would be bad for a crowded beach.

 

We are very happy with the batteries.  We have ridden nearly 3 hours on the out-of-the-box charge!

NEXT STEPS

Stay tuned for our next video where we code and breadboard the "Smarts" of the design using the MKR1000 and various sensors of the maker kit.