Skip navigation
#Blog10_A   Hello Everyone!   It's great to be chosen for the Design for a Cause' Design Challenge, I am thankful to #Element14 Community, #Arduino, and the sponsors.   Here is the Final Project demo!     I am very much thank full to prasannag1993 (Prasanna Kumar)vinyasa.mv , genebren Gene Breniman Sir, gkbhat95 ,  dixonselvan and all my friends for their encouragement and support.   The Code : // Headers for Audio Circuit #include <SD.h> #include &l ...
#Blog10   Hello Everyone!   Here is my work on Sensor data collection and using those data for decoding the gestures       The bending of the finger is denoted as 1, not bending or rest condition is denoted as 0. The analog data collected from each sensor is plotted as S0,s1..S4, and the corresponding statement for the gesture is assigned.   The analog values are made to digital using binary representation and also represented as a decimal value. The Same Algorithm ...
#Blog9   Hello Everyone!   Here is my work on generating the Audio through the available online tool.     1. A voice note or virtual voice can be created through the below link address     https://www.text2speech.org/       2. The Audio file to store on the SD card must be in the .wav format with 16000 Hz, 8-bit unsigned PCM mono quality That can be converted using below address https://audio.online-convert.com/convert-to-wav   3. Usin ...
#Blog8   Hello Everyone!   Here is my work on integrating Hand Glove to the Arduino MKR1000 Setup   Five Flex Sensor attached to each finger is interfaced through the voltage divider circuit to Analog input pins of the Arduino MKR1000   The Code   //Observe all the flex sensor reading in a tabular column void setup() {   // initialize serial communication at 9600 bits per second:   Serial.begin(9600); } void loop() {   // read the input on f ...
#Blog7   Hello Everyone!   Here is my work on the Tiny OLED Display, which is of I2C Interface.     Display: SSD1306 Type : 4 Pin 128X64 OLED Display Interface : I2C Resolution : 128 X 64 Display Size : 0.96 inch   The Circuit Diagram The Code   #include <Wire.h> #include <ACROBOTIC_SSD1306.h> void setup() {   Wire.begin();   oled.init();               &# ...
#Blog6   Hello Everyone!   Here is my work on making the Smart Glove that can sense the gestures.   . The Glove is attached with 5 Flex sensor, each for the finger placed to detect the bending of the finger to analyze the gesture.     Stay Tuned! Thanks for reading my blog... ...
#Blog5 Hello Everyone!   Happy Independence Day Its August 15, we celebrate Independence Day in our country.   Here is my work on integrating SD Card Shield and PAM8403 Audio Amplifier to Arduino MKR1000. Which is the part of  "Smart Voice Synthesizer, Visualizer". As per the design, the hand Gestures will be transformed into voice where this implementation play the key role.  Components Required Arduino MKR1000 Arduino UNO shield Arduino MKR1000 SD Card Shield PA ...
#Blog4   Hello Everyone   Getting Started with Arduino MKR 1000 Hello Everyone!   Voltage Divider Circuit to measure the Bending and a LED indication     In this below Demo, on detecting the bending of the flex sensor, a LED will glow for the indication. The program just follows the simple if else statements after reading the analog Voltage form the Voltage divider circuit.     In the Below demo, as the flex sensor bends, the LED brightness change ...
#Blog3   Hello Everyone   Got received other pending parts! Let’s begin the basic element that required to capture the Gesture. Gestures are the physical actions that convey some meaningful information. It includes movement of the hands. The primary goal is to capture the bending information of the fingers through the gesture that conveys some messages.   Hence we need a sensor that can be attached to the fingers and then it can be able to capture the bending detail ...
Hello Guys   A very special Thanks to #Element14, #Arduino and other Sponsors’ for the Challenger’s Kit. I received my kit on 15th July. Here are some photos on unboxing the Challenger’s Kit.   Image 1 : The Challenger's Kit Image 2 : Arduino MKR1000 Dev Board Image 3 : SD Card Shield, Arduino MKR1000 & UNO Shield Interface Adapter Board Image 4: Ultrasonic Sensor and other peripherals    Apart from these, the Flex Sensor & Hand Glov ...
#FirstBlogpost   Smart Voice synthesizer, visualizer and Home Automation System for Dumb & Deaf   Hello Everyone, It's great to be chosen for the Design for a Cause' Design Challenge, I am thankful to #Element14 Community, #Arduino, and the sponsors. I am writing my first blog post to introduce my project that aims to solve the challenges faced by the people who are unable to speak   According to a Statistics, the number of deaf-dumb in the world is roughly calculated to ...